3.2.2.4.2.2 Building and Loading the Project and Setting Up
Debug
Open the vienna_settings.h file, set
VIENNA_INCR_BUILD to 2.
Right click on the project name, and click Rebuild Project. The project
builds successfully. Click Run → Debug, which launches a
debugging session. In the case of dual CPU devices, if a window appears
indicating a CPU must be selected, then perform a debug. In this case, select
CPU1. The project then loads on the device, and CCS debug view becomes active.
The code halts at the start of the main routine.
To add the variables in the Watch or Expressions
window, click View → Scripting Console to open the scripting
console dialog box. On the upper right corner of this console, click on
Open to browse to the setupdebugenv_build2.js script
file, which is located inside the project folder. This file populates the
Watch window with the appropriate variables needed to debug the
system. Click the Continuous Refresh button () on the Watch
window to enable continuous update of values from the controller. Figure 3-21 illustrates the Watch window.
Figure 3-21 Build Level 2: Closed
Current Loop Expressions View
Enable real-time mode by hovering the mouse on the buttons on
the horizontal toolbar, and clicking the button.