TIDUFB8 December 2024
Figure 2-3 shows how the current input analog front end is different from voltage analog front end.
The analog front end for current consists of footprints for electromagnetic interference filter beads (FB6 and FB8), and a RC low-pass filter (R12, R21, C16, C18).
Equation 2 shows how to calculate the range of differential voltages fed to the current ADC channel for a given maximum current, and shunt resistor value.
A SHUNT value of 3mΩ is used, the input signal to the current ADC has a voltage swing of ±63.6mV, 63.6mV when the current rating of the meter (15A) is applied. This relatively low voltage, when using GAIN = 16 is well within the required Full-Scale Range of ±75mV. See also the full-scale range table in the AMC130M02 2-Channel, 64kSPS, Simultaneous-Sampling, 16-Bit, Reinforced Isolated Delta-Sigma ADC With Integrated DC/DC Converter data sheet.
GAIN SETTING | FSR |
---|---|
1 | ±1.2V |
2 | ±600mV |
4 | ±300mV |
8 | ±150mV |
16 | ±75mV |
32 | ±37.5mV |
64 | ±18.75mV |
128 | ±9.375mV |