TIDUFB8 December 2024
The MSPM0+ MCU is configured to communicate to the PC GUI through an UART interface on J12 in this reference design. The PC GUI polls data from the MSPM0G1106 using a UART module configured for 9600 baud with 8N1. The UART protocol for formatting the UART data is named DLT-645 and the UART module utilizes two DMA Channels: Channel 2 for data receive and Channel 3 for data transmit. See also the Single Phase and DC Embedded Metering (Power Monitor) Using MSP430I2040 application note.
UART data is processed in the HAL_startUARTDMAReceive()
function,
by setting a trigger at 14 bytes, as this is the byte which codes the packet length
(which can change dynamically from packet to packet). After decoding the byte 14,
the UART DMA transfer length value gets updated to a new length, which equals the
rest of the DLT-645 protocol packet, transmitted by the PC GUI.