TIDUFB8 December 2024
Figure 2-1 shows that for voltage sensing, the choice of voltage divider resistors for the voltage channel is selected to make sure the Mains voltage is divided down to adhere to the normal input ranges of the AMC130M02 device. Since the AMC130M02 ADCs have a large dynamic range and a large dynamic range is not needed to measure voltage, the voltage front-end circuitry is purposely selected so that the maximum voltage seen at the inputs of the voltage channel ADCs are only a fraction of the full-scale voltage. By reducing the voltage fed to the AMC130M02 voltage ADC, voltage-to-current crosstalk, which actually affects metrology accuracy more than voltage ADC accuracy, is reduced at the cost of voltage accuracy. For current sensing, a SHUNT resistor is selected based on the current range required for energy measurements and also the minimization of the maximum power dissipation of the shunt.
In this design, the AMC130M02 device interacts with MSPM0 MCU in the following manner: