SBAA201A March 2013 – March 2023 ADS1120 , ADS1120-Q1 , ADS1147 , ADS1148 , ADS114S06 , ADS114S06B , ADS114S08 , ADS114S08B , ADS1220 , ADS122C04 , ADS1247 , ADS1248 , ADS124S06 , ADS124S08
All trademarks are the property of their respective owners.
Resistance temperature detectors (RTDs) work by correlating the change of the resistance of a metal sensing element versus a temperature change. As the temperature of the RTD element increases, the electrical resistance of the RTD metal increases. When performing the measurement of a resistive sensor, such as an RTD in data acquisition systems, a constant current source excitation is frequently used.
The ADS1148 and ADS1248 family of devices incorporates two programmable current sources that can be used to excite the RTD sensors. Figure 1-1 shows a typical configuration used to measure an RTD in a four-wire configuration.
In the simplified circuit diagram shown in Figure 1-1 , the current from the IDAC source flows through the RTD sensor and the return current flows through the RBIAS resistor. The RLEAD resistor represents the lead wire resistance connecting the RTD element, generally limited to 10 Ω or less. The voltage generated across the RBIAS resistor is the voltage reference for the ADC. In addition, the RBIAS resistor places the RTD at a voltage greater than the analog negative supply (AVSS) in order for the sensor to be biased in the valid input common-mode voltage range of the ADC.
ADCs produce an output code as a function of the ratio of the input voltage to the reference voltage. In the ratiometric circuit shown in Figure 1-1, the voltage across the RTD sensor and the RBIAS resistor are generated with the same excitation source. Any changes as a result of the excitation current source drift is reflected across the sensor at the input path of the device, and across the RBIAS resistor at the reference path of the ADC. In this ratiometric configuration, if the RTD and RBIAS resistances remain unchanged, the digital output of the ADC is unaffected by changes of the excitation source.
Performing sensor measurements in a ratiometric configuration provides a significant advantage, where the errors as a result of the absolute accuracy of the excitation current and the errors because of to the excitation drift are virtually eliminated. In addition, when performing measurements in a ratiometric configuration, the noise of the excitation source at the inputs is reflected to the reference path of the ADC; and in this manner, the noise cancels.
In many applications, input RC low-pass filters are employed to improve the end-product immunity to radio frequency interference (RFI) and electromagnetic interference (EMI). However, it is important that the input filter and the reference filter have matched time constants or the cancellation of current source noise can degrade, leading to increasing noise with increasing signal level. Although the ratiometric circuit can work without the use of external RC filters, the addition of low-pass RC filters may prove to be beneficial in noisy environments, where the sensor circuit is prone to noise interference. This document focuses on maintaining noise cancellation of the current source when external RC filters are used.
In order for effective ratiometric cancellation to occur, the errors due to the excitation source drift and noise must be equally reflected at the inputs of the ADC, and at the reference inputs of the device. In this configuration, the excitation noise cancels, resulting in a stable, high-resolution measurement. In applications where external filters may be required to eliminate noise interference, make sure to balance the corner frequency of the reference low-pass filter to the corner frequency of the input low-pass filter.
The circuit diagram of shows a generic circuit topology frequently used in front of differential amplifiers. The input path RC low-pass filter consists of two matched series resistors, one differential capacitor, and two common-mode capacitors. This passive filter provides a first-order 20-dB/decade roll-off characteristic.
This filter topology provides attenuation for both the differential and common-mode voltage signals. The differential capacitor value is typically chosen to be at least 10 times larger than the common-mode voltage capacitors. By simple inspection, derive Equation 1 and Equation 2 to calculate the corner frequencies:
Differential-Mode Corner Frequency:
Common-Mode Corner Frequency:
When the CDIFF capacitor value is chosen to be 10 times larger than the common-mode capacitors, the resulting differential filter provides a corner frequency that is 20 times lower than the common-mode filter corner frequency. The differential signals are attenuated at a lower frequency than the common-mode signals. The internal programmable gain amplifier (PGA) of the ADS1248 tends to amplify differential signals and reject the common-mode voltage signals. Providing this ratio of capacitors helps to mitigate the effects due to the mismatch of the common-mode capacitors, where the asymmetric noise attenuation caused by the common-mode capacitor mismatch is attenuated to insignificant levels.
A similar filter topology may be applied to the RTD ratiometric measurement circuit. Make sure to match the corner frequency of the RTD filter at the input path and the corner frequency at the reference path.
The RTD sensor resistance along with the RBIAS resistor affect the time constants of the filters. In order to analyze the circuit in Figure 2-2, a zero-value time constant technique approach[1] may be used to obtain an estimate of the differential and common-mode corner frequencies involved.
Start by considering the differential filter corner frequency at the inputs of the ADC. The signal sources are set to zero by replacing the current excitation source with an open circuit, as shown in Figure 2-3. Replace differential input capacitor CIN_DIFF with a test voltage source and the rest of the capacitors with open circuits.
The effective resistance seen by the test voltage source is RTD + R1 + R2. Therefore, the RC constant seen by this filter is approximately CIN_DIFF (RTD + R1 + R2), resulting in an approximate corner frequency of:
The same approach is used to determine the corner frequencies of the common-mode filters, as shown in Figure 2-4.
When replacing CIN_CM1 with a test source, the resistance seen by CIN_CM1 is R1 + RTD + RBIAS, yielding a corner frequency of:
In similar fashion, the corner frequency provided by CIN_CM2 is given as:
The resistance of the RTD sensor changes with temperature measurement, and thus changes the frequency response of the differential filter. It also causes a mismatch on the corner frequencies of the input common-mode filters, but the impact of noise cancellation caused by the common-mode filters is not as significant as the differential filters. Scale the R1 and R2 resistors to be larger than the RTD sensor in order to help mitigate this effect.
Using the same approach, the corner frequencies for the differential reference path circuit may be calculated as:
And the common-mode filters at the reference path may be calculated as:
Although it is not always possible to exactly match the corner frequencies of all the filters, a good compromise is to attempt to balance the corner frequencies of the input path differential filter and the reference path differential filter because these filters have a dominant effect in the performance.