DAC Output Range | DAC VREFH Input Voltage | DAC VREFL Input Voltage |
---|---|---|
–5V to 5V | 5V | –5V |
High-precision digital-to-analog converters (DACs) used in applications like magnetic resonance imaging (MRI) machines and arbitrary waveform generators (AWG) generally require a high-precision voltage reference. A cause of common issues with these systems is the undesired series resistance on the reference input of the DAC. The resistance will induce a DAC input-code dependent voltage potential across them as the input current of the R-2R ladder changes based on the code. The end result is that the reference voltage will seem to change based on the DAC code, which will cause a bow shaped integrated non-linearity error curve.
To remedy this issue, high-precision DACs often feature a reference force and sense pin for each of the reference inputs (VREFH and VREFL). While these pins are essentially just two parallel connections with individual series resistance to the reference input nodes of the R-2R ladder, the addition of an external unity-gain reference buffer will allow the voltage at the node to be compensated by the amplifier. The small bias current flowing into the op amp inverting input will generate a minimum voltage across the series resistance of the sense input, while output of the op amp can source the current required by the R-2R ladder.
The DAC8871 typical output impedance of approximately 6.25kΩ, and assuming room temperature operation, has a thermal noise that can be calculated as shown in the following equation:
The reference buffer must be able to quickly source transient currents necessary for the R-2R ladder when the DAC changes codes. Given the architecture of the DAC8871, the maximum transient current would occur when the DAC transitions from zero- or full-scale code to the mid-scale. This transient is simulated with a current source between the VREFH and VREFL inputs. The following simulation shows the differential reference voltage during the current transient, simulated with the OPA828 and OPA227. This shows that the reference error magnitude and duration is reduced with the OPA828.
The total noise generated by the circuit is shown in the following simulation. The reference, inverting amplifier, and reference buffers each contribute to the noise. Note that the VREF- input has greater noise due to the contribution of the inverting amplifier and the discrete resistors in its feedback network.
Device | Key Features | Link | Other Possible Devices |
---|---|---|---|
DAC8871 | 16-bit, single-channel, serial-interface, high-voltage, bipolar-output DAC | 16-Bit Single Channel, Serial Interface, ±18V (High Voltage Bipolar) Output DAC | Precision DACs (≤10 MSPS) |
OPA828 | Low-offset, low-drift, low-noise, 45-MHz bandwidth, JFET-input operational amplifier | High-speed (45MHz and 150V/μs), 36V, low-noise (4nV/√Hz) RRO JFET operational amplifier | Precision op amps (Vos < 1mV) |
OPA221 | Low-power, 1.1nV/√Hz noise, high-performance operation amplifier | 1.1nV/rtHz Noise, Low-Power, Precision Operational Amplifier | Precision op amps (Vos < 1mV) |
REF6050 | Low-noise, high-precision, 5-V output voltage reference | 5V, 5ppm/°C high-precision voltage reference with integrated buffer and enable pin | Series voltage references |
All trademarks are the property of their respective owners.
TI PROVIDES TECHNICAL AND RELIABILITY DATA (INCLUDING DATASHEETS), DESIGN RESOURCES (INCLUDING REFERENCE DESIGNS), APPLICATION OR OTHER DESIGN ADVICE, WEB TOOLS, SAFETY INFORMATION, AND OTHER RESOURCES “AS IS” AND WITH ALL FAULTS, AND DISCLAIMS ALL WARRANTIES, EXPRESS AND IMPLIED, INCLUDING WITHOUT LIMITATION ANY IMPLIED WARRANTIES OF MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE OR NON-INFRINGEMENT OF THIRD PARTY INTELLECTUAL PROPERTY RIGHTS.
These resources are intended for skilled developers designing with TI products. You are solely responsible for (1) selecting the appropriate TI products for your application, (2) designing, validating and testing your application, and (3) ensuring your application meets applicable standards, and any other safety, security, or other requirements. These resources are subject to change without notice. TI grants you permission to use these resources only for development of an application that uses the TI products described in the resource. Other reproduction and display of these resources is prohibited. No license is granted to any other TI intellectual property right or to any third party intellectual property right. TI disclaims responsibility for, and you will fully indemnify TI and its representatives against, any claims, damages, costs, losses, and liabilities arising out of your use of these resources.
TI’s products are provided subject to TI’s Terms of Sale (www.ti.com/legal/termsofsale.html) or other applicable terms available either on ti.com or provided in conjunction with such TI products. TI’s provision of these resources does not expand or otherwise alter TI’s applicable warranties or warranty disclaimers for TI products.
Mailing Address: Texas Instruments, Post Office Box 655303, Dallas, Texas 75265
Copyright © 2024, Texas Instruments Incorporated