The purpose of this study is to characterize the effects of heavy-ion irradiation on the single-event latch-up (SEL) performance of the ADC168M102R-SEP, dual 16-bit analog-to-digital converter (ADC). Heavy- ions with an LETEFF of 48MeV-cm2/mg were used to irradiate the devices with a fluence of 1 × 107 ions/cm2. The results demonstrate that the ADC168M102R-SEP is SEL-free up to LETEFF = 48MeV-cm2/mg at 125°C.
All trademarks are the property of their respective owners.