SBAU472 December 2024 TMAG5170 , TMAG5170-Q1 , TMAG5173-Q1 , TMAG5273
This document serves to accompany the design files for the ROTATEPUSH-MAG-ACC attachment for the magnetic sensing evaluation kits (EVMs) that interface with TI-SCB such as the TMAG5170UEVM. In addition to this guide, the design files are provided as an example and may be used in a 3D printer to generate a demonstration of common functions of angle measurement and push button functionality using a three-dimensional Hall-effect sensor.
Design files described in this document can be downloaded from Rotate and Push Module design files.
All trademarks are the property of their respective owners.
This ROTATEPUSH-MAG-ACC attachment uses an N42 grade cylindrical magnet as a magnetic field source to demonstrate the ability of magnetic sensors to track rotational and push button motion of a nearby magnet. The magnet is glued into a 3D-printed knob object, which can rotate freely about the 3D-printed base. The knob can also be pressed and return back to the starting position due to the spring. More details about this function are described in Using Hall-Effect Sensors for Contactless Rotary Encoding and Knob Applications and 3D Hall-Effect Sensor for Knobs in Appliances.
Examples of expected magnetic field data captured using the TMAG5173EVM are shown in Figure 1-1.
Nylon components were selected as these components are non-magnetic and do not interfere with the magnetic field and bond well when glued.
This function can be further explored using the angle encoding reference design in the TI Magnetic Sense Simulator tool (TIMSS) available at https://webench.ti.com/timss/.