7-segment displays are simple LED configurations that display single numerical characters and a limited selection of letters, such as can be found in digital clocks, microwaves, or calculators. Typically, in these devices, multiple 7-segment displays are used to display a multi-digit number, with each 7-segment display showing one number.
Each 7-segment display has at least 8 inputs – one for each LED, and a power input. Circuits using multiple 7-segment displays need progressively more inputs for each display used. If each input were controlled directly by a microcontroller, this can use at least 28 GPIO pins for a simple 4-digit clock. To reduce the GPIO requirements, IO expander such as shift registers can be used to control multiple display inputs using fewer microcontroller outputs.
TI programmable logic devices (TPLD) can be used to integrate IO expansion function with control logic before outputting to a 7-segment display. This allows designers reduce the necessary size and function of the MCU.
One method of controlling a 7-segment display using fewer IO pins is I2C addressing. Some devices within the TPLD portfolio such as the TPLD1202 have integrated I2C registers that can be programmed using an MCU. These internal registers can be connected to the TPLD IOs to drive a 7-segment display. The configuration of an I2C block in InterConnect Studio is shown in Figure 1.
Multiple TPLDs can be configured with different I2C addresses and connected to the same I2C input to allow for further GPIO expansion. Each TPLD can either be configured with a different I2C address, or can have a different I2C address set through hardware. This allows for control of multiple 7-segment displays using only 2 I2C pins from the MCU, as shown in Figure 2.
Another method of controlling a 7-segment display using fewer IO pins is to use the TPLD’s state machine. This allows for less direct control of a 7-segment display than using the I2C method, as the MCU cannot directly write to the 7-segment display, but can allow the TPLD to control the display less external direction. Figure 3 shows a configuration that uses the state machine to display a count down from 3 that reduces after a triggering signal is sent. Unlike the I2C method, this configuration requires only a single external line and does not need to be in any communication protocol.
This method also allows for more complex designs using the internal logic elements of the TPLD, such as the controller shown in Figure 4. In this design, when an input signal is sent, the devices sets the display to output “3” and counts down to 0 over the course of 3 seconds.
Advantages of TPLD in controlling a 7-segment display include:
These advantages are exemplified in the configuration shown in Figure 5. In this configuration, the 7-segment display is directly controlled by I2C, but after 5 seconds of no new I2C command being received, the display can instead cycle through the message “NO I2C” until a new I2C command is sent.
TPLD allows for the integration of multiple logic and signal handling blocks into a single device. This can reduce the total design size while also offering new capabilities for designers to utilize. For more information on TPLD, visit the TPLD1201 product page or ask our engineers a question on the TI E2E™ Logic Support Forum.
All trademarks are the property of their respective owners.