All trademarks are the property of their respective owners.
Most RF antenna systems feature power amplifiers (PA) for their transmitter design. These antenna systems include:
Power amplifier biasing circuits are implemented in these systems to ensure two things: first, that the power output of the amplifier is known and controlled, and second, that the system is powered on and off safely to reduce the risk of damaging the PA. Power amplifiers are commonly created with either gallium nitride (GaN) or laterally diffused MOSFET (LDMOS) transistors. Power output in both GaN and LDMOS FETs (field-effect transistors) is dependent on the current that flows through the device from the drain to the source (IDS).
The IDS current is determined by a few variables: the drain voltage (VD), the gate voltage (commonly called VGS), and temperature. Figure 1-2 shows an example of IDS values against the drain voltage for a selection of VGS voltages for a GaN FET. The higher VGS voltages result in a higher IDS, or more power from the amplifier. When the VGS voltage is sufficiently low, the FET allows virtually zero IDS current. This VGS voltage is called the pinch-off voltage. IDS is also dependent on the drain voltage, but most designers do not vary the VD. Instead, designers use optimized VD voltages for the desired power levels. The VD values are usually about 50 V for GaN FETs and 28 V for LDMOS FETs.
The IDS also depends on the temperature of the FET. The IDS variations due to thermal drift create the need to compensate by adjusting one of the other two variables in the system: VD or VGS. It is easier to adjust VGS, as only small voltage changes are required. Conversely, VD needs to change significantly if the device is operating in the flat areas of Figure 1-2, making it infeasible to compensate for the thermal drift by adjusting VD.
Figure 2-1 shows VGS needs to be adjusted to ensure a static IDS. Applications utilizing these FETs require this kind of compensation to ensure that the power of the antenna system is tightly controlled. VGS compensation can be implemented by either measuring the temperature of the FET, or measuring the IDS using a current shunt and adjusting the VGS accordingly.
Powering the FET on and off in a controlled routine is necessary to prevent the VGS voltage from being too high when the VD is applied. Such a state causes the FET to operate in saturation mode, and thermal damage the FET or board that it is mounted on. Powering on a FET requires the following steps:
The PA can be safely shut down by reversing the power-on steps.