Digital isolators are integrated devices used to isolate digital signals and transfer digital communication across an isolation barrier. Digital isolators are often expected to withstand hostile electrical conditions in order to protect human users and sensitive equipment. Ideally this is done so the isolator appears invisible to the protected circuit, relaying information without adding complexity. In reality, all electrical components have an impact on the system. Electromagnetic compatibility (EMC) refers to the ability of equipment to function properly in its electromagnetic environment. Knowing how a digital isolator performs in terms of EMC allows a system designer to select devices that generate minimal unwanted radiated emissions while providing reliable protection from received electromagnetic energy such as ESD and EFT.
Electromagnetic interference (EMI) is an induced disturbance in an electrical circuit caused by an external electromagnetic field. Because EMI depends on many factors and is difficult to accurately predict, it is important to minimize known sources of interference during circuit design and layout. Radiated emissions are a type of EMI which refers to mid-to-high frequency noise produced by a device while operating under normal conditions. International standard EN55032:2010 requires radiated emissions testing be conducted between 30 MHz to 1 GHz and up to 6 GHz depending on a device’s internal oscillator frequency. For the test described in this common industrial standard, the equipment under test (EUT) is placed 10 meters away from the measurement antenna in an anechoic chamber as shown in Figure 1-1 below.
With the equipment operating normally, the antenna measures received emissions in dB µV/m over the range of tested frequencies. To pass this standard test, measurements must remain below defined thresholds, shown in Table 1-1, for all measured frequencies.
Frequency (MHz) | Limit (dBuV/m) |
---|---|
30 - 230 | 30 |
230 - 1000 | 37 |
It is important that the equipment under test is powered and operating under normal conditions (as would be seen in the equipment’s final use case) while conducting radiated emissions measurements. Emissions vary depending on device configuration and power usage, thus testing should be completed to reflect the worst-case operating conditions for emissions. Carefully selecting equipment’s supply voltages, communication data rates, and device variants can help a system designer reduce overall emissions.
The amount of energy present in a radiated electromagnetic field is proportional to the energy contained in the original conducted signal. This means that by reducing the energy in a communication signal, less energy will be radiated into the environment. Using lower supply voltages for signaling devices where possible will help reduce these energies.
As data rate increases, parasitic capacitive loads charge and discharge more often, increasing the overall average current. For this reason, higher data rate signals and their harmonics can appear in emissions measurements which can cause interference in other parts of the system. Similarly the fast slew rate required for such rates contain high frequencies that can also contribute to emissions. Figure 1-2 and Figure 1-3 show the radiated emissions performance of TI’s ISO7741 device at two different data rates. In both cases, ISO7741 devices show significant margin to CISPR32's limit line.
Operating devices at lower data rates and using devices with slower slew rates (rated at lower data rates) can reduce the amount of high frequencies present in a system and reduce emissions from these harmonics. In systems where lowering data rate is not desired or possible, designers may optimize PCB layout, place strategic impedances, and use EMC shielding methods to reduce the impact of the high frequencies on emissions.
ESD testing is conducted to measure how much electrostatic discharge stress a device or equipment can withstand before becoming inoperable. The JEDEC standard provides device-level tests to model different energy sources, including the human body model (HBM), charged device model (CDM), and machine model (MM) – waveforms for which can be seen in Figure 4. IEC 61000-4-2 offers a similar standard test for equipment-level tests. These standards model high-current, short-duration strikes to represent the characteristics of a real discharge event. Each test is conducted up to a peak test voltage to characterize the level a device or system can withstand. Example values for IEC 61000-4-2 are shown in Table 1-2.
Level | Contact Discharge | Air Discharge |
---|---|---|
Test Voltage (+- kV) | Test Voltage (+- kV) | |
1 | 2 | 2 |
2 | 4 | 4 |
3 | 6 | 8 |
4 | 8 | 15 |
ESD protection and immunity is a consideration for many devices, but protection for isolators proves to have its own challenges. Non-isolated ESD test methods stress supply and data lines with respect to the local ground. Typical protection methods such as TVS diodes provide a safe path to ground for the energy in ESD strikes. Because isolated systems have separate grounds, TVS diodes cannot provide protection in the same way. This is because the energy in an across-the-barrier strike is presented as common mode to “single-side” or “local” ESD protection. A local TVS diode would not clamp due to a large voltage difference between isolated ground planes.
Some industries require equipment to provide a certain level of ESD immunity for user safety and product longevity. The simplest method of increasing system-level ESD capabilities is to choose robust devices with high individual ESD ratings. As shown in Figure 5 below, TI’s ISO77xx family has the highest level of ESD protection among similar devices, reducing the number of external components needed for system protection. When even higher levels are required, external components such as Y-capacitors and gas discharge tubes (GDT) may be used to attenuate and dissipate energy from a discharge. Though external solutions can provide extra protection, they may add cost, board size, or operational constraints.
Like ESD testing and ratings, EFT ratings are a measure of device and equipment robustness, but with a different focus on cause and system impact. Switching-transients from inductive loads or relay-contact-bounce present stresses that are less likely to cause device damage than ESD strikes, but may instead interrupt normal system behavior. These transients are thus simulated differently under IEC 61000-4-4, shown in Figure 1-6 below, which models short rise-time, repetitive, low energy pulses to challenge system performance under such disruptive conditions. Similar to ESD, these tests are conducted up to a specified voltage level like shown in Table 1-3.
Level | On Power Port, PE | On I/O, Data and Control Ports |
---|---|---|
Test Voltage (kV) | Test Voltage (kV) | |
1 | 0.5 | 0.25 |
2 | 1 | 0.5 |
3 | 2 | 1 |
4 | 4 | 2 |
EFT events may occur on power and ground lines from switching loads or on signal lines from relay bounce or other induced-switching transients. Both injection types can cause glitches in an associated signal line. This could appear as a bit error and may result in data corruption or system lock-up. To reduce the risk of these failures, robust devices rated to resist such transients may be selected for use in a design. External filtering components such as decoupling capacitors, RC networks, and common-mode chokes may also be used to attenuate high frequency switching noise seen by a susceptible device. Figure 1-7 below shows the high EFT resiliance provided by TI's ISO77xx family compared to what is offered by similar competitor devices. These test levels were achieved with 0 bit errors.
This document describes how electrical components can interact with their electromagnetic environment and how negative interactions can be limited. Selecting devices that provide reliable protection from received electromagnetic energy and minimize unwanted radiated emissions is a fundamental way to increase a system's EMC performance and meet standard requirements. This, combined with EMC mitigation techniques, ensures correct operation of equipment in different electromagnetic environments. Texas instrument’s ISO77xx family of digital isolators offers industry leading EMC performance with minimal radiated emissions while operating robustly under ESD and EFT disturbances.
TI PROVIDES TECHNICAL AND RELIABILITY DATA (INCLUDING DATASHEETS), DESIGN RESOURCES (INCLUDING REFERENCE DESIGNS), APPLICATION OR OTHER DESIGN ADVICE, WEB TOOLS, SAFETY INFORMATION, AND OTHER RESOURCES “AS IS” AND WITH ALL FAULTS, AND DISCLAIMS ALL WARRANTIES, EXPRESS AND IMPLIED, INCLUDING WITHOUT LIMITATION ANY IMPLIED WARRANTIES OF MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE OR NON-INFRINGEMENT OF THIRD PARTY INTELLECTUAL PROPERTY RIGHTS. |
These resources are intended for skilled developers designing with TI products. You are solely responsible for (1) selecting the appropriate TI products for your application, (2) designing, validating and testing your application, and (3) ensuring your application meets applicable standards, and any other safety, security, or other requirements. These resources are subject to change without notice. TI grants you permission to use these resources only for development of an application that uses the TI products described in the resource. Other reproduction and display of these resources is prohibited. No license is granted to any other TI intellectual property right or to any third party intellectual property right. TI disclaims responsibility for, and you will fully indemnify TI and its representatives against, any claims, damages, costs, losses, and liabilities arising out of your use of these resources. |
TI’s products are provided subject to TI’s Terms of Sale (www.ti.com/legal/termsofsale.html) or other applicable terms available either on ti.com or provided in conjunction with such TI products. TI’s provision of these resources does not expand or otherwise alter TI’s applicable warranties or warranty disclaimers for TI products. |
Mailing Address: Texas Instruments, Post Office Box 655303, Dallas, Texas 75265
Copyright © 2020, Texas Instruments Incorporated |