The Controller Area Network (CAN) protocol is popular in power delivery, grid infrastructure, motor drives, factory and building automation applications due to its arbitration and prioritization features. Since many of these applications feature multiple voltage domains, galvanic isolation is needed along the signal path in these CAN networks. Engineers can isolate their CAN signals through devices with integrated isolated CAN transceivers or with a discrete digital isolator placed next to the CAN transceiver, which provides the necessary protection of the low voltage circuitry from the high voltage side. These devices also improve noise immunity and ensure reliable communication between the CAN nodes on the different voltage domains.
However, isolating the signal path is only one challenge associated with communicating across different voltage levels. Isolators and isolated CAN transceivers require isolated power supplies to function properly. In some limited instances, both sides of the isolating device can be powered directly from the system power supply that exists in the two domains. More commonly, however, the isolated CAN transceivers from one board are likely communicating with a transceiver on a distant board, and hence the need to provide a local isolated power supply becomes inevitable.
This application brief shares the different options to isolate signal and power in isolated CAN systems. Figure 1-1 shows four different isolated CAN nodes. Moving from node 1 to node 4, each solution has different level of integration. Node 1 has a complete discrete solution with the discrete isolator in series with a CAN transceiver, while the transformer driver provides the excitation for the external transformer to provide the isolated power supply (VISO1). Node 2 uses a similar isolated power supply but shows the integrated isolated CAN devices that save some board space.
Node 3 uses an isolated data and power device (ISOW7741) to eliminate the digital isolator and the isolated power discrete components from node 1. The external CAN transceiver in series allows for CAN communication. Finally, Node 4 integrates the CAN transceiver in the isolated data and power device to further simplify the design.
The discrete solutions used for Node 1 and Node 2 do have their advantages. The efficiency of power transfer is around 90% and the radiated emissions are relatively lower due to the lower switching frequency of the transformer drivers (150kHz to 420kHz). The flexibility of choosing any CAN transceiver to meet the system requirements allows Nodes 1 and 3 to be unique. But there are several reasons why the completed integrated solution of Node 4 still receives the approval from many designers.
Integrating the planar transformer in a package comes with its challenges. The driver circuit, transformer and the receiver all need to be matched well so there is no common mode noise produced by the isolated power circuitry. In addition, since the size of the transformers needs to be kept small, this drives the switching frequencies to be limited in the MHz range. The faster switching frequency causes more noise in the system.
TI’s isolated CAN transceiver, the ISOW1044, uses a symmetric architecture of the isolated power design to improve the emissions performance of these devices over competing solutions. Figure 1-3 shows the test setup of the ISOW1044 radiated emissions. A battery voltage source was used with a low-dropout regulator (LDO) to generate the 5-V power supply for the ISOW1044 on an evaluation module. Ferrite beads were used for the testing before and after the LDO and also between the output of the ISOW1044 and ground to suppress high amplitude spikes in the emissions spectrum.
Figure 1-4 shows the ISOW1044 passing the CISPRS32 class B standard limits on a two-layer PCB without any stitching capacitors, Y-capacitors or common mode choke (CMC) at the CAN data-rate of 1 Mbps.
Packing multiple die inside a single chip does add the challenge of thermal performance of the integrated device. The ISOW1044 and a competing device were both tested under the same conditions at CAN with Flexible Data Rate (FD) speed of 5 Mbps and the thermal images were captured by a thermal gun. The results shown in Figure 1-5 where the top image refers to the ISOW1044 and has a maximum temperature of 39.3 °C. A competing device is also shown in Figure 1-5 and is running 6.2°C hotter than the ISOW1044. 47% efficiency of the ISOW1044 enables lower power dissipation and extends the ambient temperature range support from -40C to 125C.
Fully integrated ISOW1044 guarantees the CAN FD timing specs up to 5 Mbps in one single data sheet, eliminating uncertainty caused by stringing together multiple components. ISOW1044 also features extended bus fault protection of up to +/-58V, providing extra margin to protect against accidental CAN bus shorts to power supplies. In addition, the integrated 10 Mbps GPIO channel can be used for additional system-level signal isolation eliminating the potential need for additional opto-coupler or digital isolator. ISOW1044 can operate from a single 5 V supply or have the option to use a separate logic supply that can go down to 1.8 V.
TI’s isolated CAN transceiver with integrated DC-DC converter, ISOW1044, provides a compact solution as compared to discrete solution available in the market. The device passes the CISPR32 class B radiated emissions and is highly efficient to enable operation over the entire industrial temperature range.
TI PROVIDES TECHNICAL AND RELIABILITY DATA (INCLUDING DATASHEETS), DESIGN RESOURCES (INCLUDING REFERENCE DESIGNS), APPLICATION OR OTHER DESIGN ADVICE, WEB TOOLS, SAFETY INFORMATION, AND OTHER RESOURCES “AS IS” AND WITH ALL FAULTS, AND DISCLAIMS ALL WARRANTIES, EXPRESS AND IMPLIED, INCLUDING WITHOUT LIMITATION ANY IMPLIED WARRANTIES OF MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE OR NON-INFRINGEMENT OF THIRD PARTY INTELLECTUAL PROPERTY RIGHTS. |
These resources are intended for skilled developers designing with TI products. You are solely responsible for (1) selecting the appropriate TI products for your application, (2) designing, validating and testing your application, and (3) ensuring your application meets applicable standards, and any other safety, security, or other requirements. These resources are subject to change without notice. TI grants you permission to use these resources only for development of an application that uses the TI products described in the resource. Other reproduction and display of these resources is prohibited. No license is granted to any other TI intellectual property right or to any third party intellectual property right. TI disclaims responsibility for, and you will fully indemnify TI and its representatives against, any claims, damages, costs, losses, and liabilities arising out of your use of these resources. |
TI’s products are provided subject to TI’s Terms of Sale (www.ti.com/legal/termsofsale.html) or other applicable terms available either on ti.com or provided in conjunction with such TI products. TI’s provision of these resources does not expand or otherwise alter TI’s applicable warranties or warranty disclaimers for TI products. |
Mailing Address: Texas Instruments, Post Office Box 655303, Dallas, Texas 75265
Copyright © 2020, Texas Instruments Incorporated |