PMBus is a trademark of SMIF, Inc..
All trademarks are the property of their respective owners.
The PWR784EVM evaluation module uses the TPS549D22 device. The TPS549D22 is a highly integrated synchronous buck converter that is designed for up to 40-A current output.
The PWR784EVM is designed as a single output DC-DC converter that demonstrates the TPS549D22 in a typical low-voltage application while providing a number of test points to evaluate the performance. It uses a nominal 12-V input bus to produce a regulated 1-V output at up to 40-A load current.