This technical reference manual discusses the modules and peripherals of the BQ28Z620 device, and how each is used to build a complete battery pack gas gauge and protection solution. This manual details the differences between the BQ28Z610-R2 firmware, as described in the BQ28Z610-R2 Technical Reference Manual, and the BQ28Z620 firmware. For BQ28Z620 electrical specifications, see the BQ28Z620 1-Cell to 2-Series Cell Li-Ion Battery Pack Manager Data Sheet.
The following notation is used if SBS commands and data flash (DF) values are mentioned within a text block: