All trademarks are the property of their respective owners.
This document contains information for DRV8873H-Q1 (HTSSOP(24) package, HW variant) and DRV8873S-Q1 (HTSSOP(24) package, SPI variant) to aid in a functional safety system design. Information provided are:
DRV8873-Q1 was developed using a quality-managed development process, but was not developed in accordance with the IEC 61508 or ISO 26262 standards.
Figure 1-1 shows the functional block diagram for the HW variant of this device as a reference.
Figure 1-2 shows the functional block diagram for the HW variant of this device as a reference.