Motor stall detection is crucial for many applications and is important for several reasons. First, motor stall detection helps detect when the motor reaches end of travel or when it suddenly stops due to an obstruction. For example, a deadbolt of an electric door lock reaching the closed position causes the motor to stall. Second, stall detection can help minimize long term damage to the motor and the mechanical system from excessive heat, wear, and stress, which occurs when a motor is overdriven when stalling. Lastly, stall detection improves efficiency and reduces power consumption by avoiding unnecessary energy consumption. Some examples of applications that benefit from motor stall detection include vacuum robots, electric door locks, and portable printers.
Today, methods exist for detecting when a brushed DC (BDC) motor stalls. These include, measuring the motor current, back EMF, and using encoders and hall sensors to monitor the position of the motor. All of these methods require some level of discrete circuitry and software implementation which increases the design cost and design size of the PCB. In this application brief, a fully integrated and intelligent stall detection design is presented that can replace discrete designs. This design is integrated in TI’s latest DRV8213 motor driver.
One of the most common methods for detecting stall in a BDC motor is by measuring the motor current. The motor current is measured using a sense resistor in series with the motor current path. The sense resistor generates a voltage across the motor that is proportional to the motor current. This sense resistor voltage is fed into an amplifier network to boost the voltage to be within the ADC dynamic range of the MCU. The MCU monitors the current sense output and detects when the current exceeds a certain threshold (VREF). When a BDC motor stalls, the current increases significantly. The threshold must be set higher than the steady state current and must be experimentally determined for the specific motor and application.
When the sense voltage exceeds VREF, a stall is detected and the MCU can perform the desired response, such as stopping the motor, reversing motor direction, or alerting the user. Figure 1 shows a high-level block diagram for this design.
The threshold value (VREF) depends on the specific motor and application. Experiments with different values and operating conditions can be required to find the threshold that covers worst cases such as when the motor is fully loaded or when operating at high or low temperatures. The sense resistor must be rated for the maximum current expected in the system.
BDC motors have high inrush currents during startup due to the high torque required to overcome moments of inertia to begin spinning. Therefore, the MCU must ignore the current during the inrush period to avoid false stall detection. This can be achieved by simply adding a delay or blanking time from when the threshold is exceeded to when the MCU reports the stall condition. The delay time is experimentally determined for each motor and application. Figure 2 shows this design using a real motor from start-up to a stall condition.
The DRV8213 integrates a stall detection method that relies on constant current monitoring similar to the discrete design mentioned in the previous section. The integrated current sensing on the DRV8213 has a current output that is proportional to the motor current. This proportional current is called IPROPI. Figure 3 shows the current sensing and regulation block of the DRV8213. The integrated current sense block is a current mirror circuit with the scalar factor. The scaled down current flows through an external resistor generating the voltage. This voltage is compared to an external VREF voltage. The VREF voltage has two purposes in the DRV8213. The VREF voltage is used to set the current regulation limit and the stall detection limit. Once the exceeds, stall detection is detected by the driver if it has been enabled.
The DRV8213 addresses the false stall detection problem during start-up by including an adjustable blanking time, TINRUSH. The DRV8213 has a TINRUSH pin where an external capacitor (CINRUSH) can be connected to GND. This pin sets the amount of time that the stall detection scheme ignores the inrush current during motor start-up. The is shown by the formula: TINRUSH = 6.5x106 * CINRUSH
Figure 4 shows more information regarding the stall detection operation. The inrush current is regulated to the ITRIP threshold. The stall detection scheme ignores this inrush current for a time set by TINRUSH. Once the motor stalls, the current rises again and this time the driver flags a stall detection by setting the nSTALL pin logic LOW to indicate a stall is detected.
The driver has three response settings for when a stall has been detected. The setting is set by the SMODE pin. The settings are as follows:
The third setting is to be used in the case that providing external voltage to the VREF pin is not possible or not desired. The internal reference voltage is fixed at 510 mV.
To conclude, the advantages of the DRV8213 design are lower overall design cost and PCB design size because the design is fully integrated to the IC. The small footprint free some space on the PCB allowing for more features to be added or to minimize the PCB size for size constrained applications. The built-in intelligence (such as the TINRUSH blanking time and the programmable stall detection response) eliminates the need for an external MCU. To learn more about the DRV8213, visit the DRV8213, product page.
TI PROVIDES TECHNICAL AND RELIABILITY DATA (INCLUDING DATASHEETS), DESIGN RESOURCES (INCLUDING REFERENCE DESIGNS), APPLICATION OR OTHER DESIGN ADVICE, WEB TOOLS, SAFETY INFORMATION, AND OTHER RESOURCES “AS IS” AND WITH ALL FAULTS, AND DISCLAIMS ALL WARRANTIES, EXPRESS AND IMPLIED, INCLUDING WITHOUT LIMITATION ANY IMPLIED WARRANTIES OF MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE OR NON-INFRINGEMENT OF THIRD PARTY INTELLECTUAL PROPERTY RIGHTS.
These resources are intended for skilled developers designing with TI products. You are solely responsible for (1) selecting the appropriate TI products for your application, (2) designing, validating and testing your application, and (3) ensuring your application meets applicable standards, and any other safety, security, or other requirements. These resources are subject to change without notice. TI grants you permission to use these resources only for development of an application that uses the TI products described in the resource. Other reproduction and display of these resources is prohibited. No license is granted to any other TI intellectual property right or to any third party intellectual property right. TI disclaims responsibility for, and you will fully indemnify TI and its representatives against, any claims, damages, costs, losses, and liabilities arising out of your use of these resources.
TI’s products are provided subject to TI’s Terms of Sale (www.ti.com/legal/termsofsale.html) or other applicable terms available either on ti.com or provided in conjunction with such TI products. TI’s provision of these resources does not expand or otherwise alter TI’s applicable warranties or warranty disclaimers for TI products.
Mailing Address: Texas Instruments, Post Office Box 655303, Dallas, Texas 75265
Copyright © 2023, Texas Instruments Incorporated