PCIe is a registered trademark of PCI-SIG.
All trademarks are the property of their respective owners.
In recent years, the automotive industry has witnessed an impressive growth in computing throughput as data integration, machine-learning (ML), and artificial intelligence (AI) have become an integral part of the automotive ecosystem. According to a 2020 report by Global Market Insights, the market size for advanced driver assistance systems (ADAS) is expected to grow from a $35 billion industry in 2019 to over $60 billion by 2026 with >10% compound annual growth rate (CAGR). Such significant expansion is attributed to increasing vehicle safety regulations and driver assistance capabilities as vehicles reach full autonomy. With the onset of 5G networks revolutionizing vehicle-to-everything (V2X) connectivity for connected car applications, computing needs will further increase to enhance vehicle connectivity. Gone are the days of electronic control units (ECUs) that perform a singular function in an isolated environment. Today’s vehicles resemble data centers on wheels comparable to traditional High-Performance Computing (HPC) platforms deployed in enterprise servers.
As Original Equipment Manufacturers (OEMs) and Tier-1s prepare to support technological advances in both ADAS and vehicle connectivity, they are rethinking the automotive data backbone architecture. Rather than rely on computing to be implemented based on domains (for example, ADAS domain), future automotive data backbones are shifting from domain to zonal architectures. This is accomplished by incorporating local computing nodes, or zone controllers, to connect ECUs and interfaces based on location within their zone, regardless of their respective domain. These zone controllers then connect to a powerful central compute node that handles the data accordingly. The value of the zonal architecture approach is three-fold:
In zonal automotive architectures, high-speed interfaces are required that enable both high bandwidth and low latency. In situations where safety-critical real-time processing is implemented, ultra-low latency becomes a must-have requirement. Fortunately, there is no need to re-invent the wheel when seeking an appropriate interface for these applications. The Peripheral Component Interconnect Express (PCIe®) ecosystem has successfully met the high bandwidth, ultra-low latency performance demands in industrial data centers, and this interface is well-suited to be used in a similar fashion for the automotive industry.
PCIe is not new to automotive. In fact, PCIe has an extensive history as an intra-ECU, board-to-board interface between processors and automotive network interface cards (NICs) for years.
There are several key advantages to using PCIe: