A heat meter is a device which measures thermal energy by measuring the flow rate and the change of temperature between the inlet and outlet of the system. These devices are very commonly found in both industrial plants to measure boiler outputs and in residential heating and cooling systems to measure the heat delivery.
Since the measurement of thermal energy requires both flow rate and temperature, it is imperative that they be measured accurately. Accuracy is important because an inaccurate measurement can result in under billing or over billing.
To avoid measurement errors, a resistance temperature detector (RTD) is commonly used. An RTD is a passive component whose resistance changes with temperature. RTDs are made using metals—such as platinum, copper, or nickel—and support a wide temperature range (approximately –200°C to +850°C). The accuracy of a Platinum RTD is defined by its class. The IEC/EN60751 standard defines four RTD classes—Class C, B, A, and AA—where Class C is the least accurate and Class AA is the most accurate. The lower accuracy classes will have a larger temperature range. For example, a Class C thin-film RTD covers the temperature range of –50°C to +600°C, while a Class AA thin-film RTD covers the temperature range of 0°C to +150°C.
Most RTD applications use a current source to excite the RTD element and create a voltage difference across the RTD, as shown in Figure 1. This voltage is proportional to the resistance of the RTD and the excitation current. The voltage potential is amplified, converted to a digital output by an ADC, and then fed into an MCU where a lookup table is used to convert the digital output to temperature.
SPACER
SPACER
RTDs in Heat Meters
Solid-state heat meters are gaining popularity in heat energy billing for residential and industrial users. These meters come with both flow measurement on either the inlet or outlet pipe and a pair of matched RTD temperature probes on both inlet and outlet pipes. Figure 2 shows a block diagram of a heat meter system using RTDs.
Low-power and high-accuracy RTDs in heat meters are desired because heat meters are standalone, battery-powered systems in most residential units. The system’s ability to quickly wake from power-off mode, sample the RTD temperature, and return to power-off mode extends battery life and minimized energy consumption.
However, these system require that the RTDs are well-matched and have matched traces to read the differential measurement correctly. At the same time, the system cost and complexity requires careful design consideration and costly calibration. High-accuracy digital temperature sensors like the TMP117 can provide a cost-optimized, yet equally accurate replacement for RTDs.
Replacing RTD With TMP117 Digital Temp Sensors
The TMP117 is a digital temperature sensor designed for low-power, high-accuracy applications. The device provides a 16-bit temperature result with a resolution of 0.0078°C, along with a typical factory-calibrated accuracy of ±0.1°C across –20°C to +50°C with a maximum accuracy specification of ±0.3°C over the temperature range of –55°C to +150°C, which exceeds the accuracy of a Class AA RTD in the same range.
Figure 3 illustrates the accuracy specification of the TMP117 vs an RTD. The graph clearly shows that accuracy specification for the TMP117 can easily outperform that of a Class AA RTD.
The TMP117 features a shutdown mode where the device aborts the active running conversion and enters a low-power shutdown mode where it typically consumes 250 nA of current. It can perform quick, 15.5-ms temperature conversions using the one-shot conversion mode an active current as low as 3.5 μA for a duty cycle of 1 Hz. After completing a one-shot conversion, the device returns to low-power shutdown mode.
Also, the device features an offset register that automatically applies a user-defined offset to the measurement results prior to an MCU read. As the TMP117 provides additional simplicity over an RTD, it eliminates the need for costly calibration, external circuitry, matched traces, and Kelvin connections easing the system designers task for accurate measurement.
Finally the TMP117 features a fast mode (400 kHz) I2C communication. These specs make the TMP117 excellent for low-power consumption requirements, as well as quick power on-off cycling necessary in Heat Meter systems.
The TMP117, with a comparable accuracy as the Class AA thin-film RTD while consuming only a fraction of the power required for temperature measurement, is designed for a variety Heat Meter applications.
Figure 4 shows the same block diagram of Heat Meter system using the TMP117 to replace the RTDs. By using the TMP117 instead of an RTD, designers can simplify both their software and system architecture to save time, board space, and costs.
Overall, the high-accuracy TMP117 temperature sensor with digital interface, fast conversion, and extremely low-power shutdown mode eliminates the need for multiple narrow-tolerance discrete components and integrated devices, which can save PCB space, complexity, and cost in Heat Meters.
COLLATERAL | DESCRIPTION |
TMP117 | ±0.1°C Accurate Digital Temperature Sensor with Integrated NV Memory |
TMP116 | ±0.2°C Accurate Digital Temperature Sensor with Integrated NV Memory |
Application Report | RTD Class-AA Replacement With High-Accuracy Digital Temperature Sensors in Field Transmitters |
Application Report | Replacing Resistance Temperature Detectors With the TMP116 Temp Sensor |
Application Report | Precise Temperature Measurements with TMP116 |
TI PROVIDES TECHNICAL AND RELIABILITY DATA (INCLUDING DATASHEETS), DESIGN RESOURCES (INCLUDING REFERENCE DESIGNS), APPLICATION OR OTHER DESIGN ADVICE, WEB TOOLS, SAFETY INFORMATION, AND OTHER RESOURCES “AS IS” AND WITH ALL FAULTS, AND DISCLAIMS ALL WARRANTIES, EXPRESS AND IMPLIED, INCLUDING WITHOUT LIMITATION ANY IMPLIED WARRANTIES OF MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE OR NON-INFRINGEMENT OF THIRD PARTY INTELLECTUAL PROPERTY RIGHTS. |
These resources are intended for skilled developers designing with TI products. You are solely responsible for (1) selecting the appropriate TI products for your application, (2) designing, validating and testing your application, and (3) ensuring your application meets applicable standards, and any other safety, security, or other requirements. These resources are subject to change without notice. TI grants you permission to use these resources only for development of an application that uses the TI products described in the resource. Other reproduction and display of these resources is prohibited. No license is granted to any other TI intellectual property right or to any third party intellectual property right. TI disclaims responsibility for, and you will fully indemnify TI and its representatives against, any claims, damages, costs, losses, and liabilities arising out of your use of these resources. |
TI’s products are provided subject to TI’s Terms of Sale (www.ti.com/legal/termsofsale.html) or other applicable terms available either on ti.com or provided in conjunction with such TI products. TI’s provision of these resources does not expand or otherwise alter TI’s applicable warranties or warranty disclaimers for TI products. |
Mailing Address: Texas Instruments, Post Office Box 655303, Dallas, Texas 75265
Copyright © 2019, Texas Instruments Incorporated |