• Menu
  • Product
  • Email
  • PDF
  • Order now
  • LM2738 Step-Down Converter Evaluation Module User's Guide

    • SNVA341B April   2008  – December 2021 LM2738

       

  • CONTENTS
  • SEARCH
  • LM2738 Step-Down Converter Evaluation Module User's Guide
  1.   Trademarks
  2. 1Introduction
  3. 2Operating Conditions
  4. 3PCB Layout - WSON
  5. 4PCB Layout - MSOP-PowerPAD
  6. 5Additional Circuit Configuration Schematics
  7. 6Revision History
  8. IMPORTANT NOTICE
search No matches found.
  • Full reading width
    • Full reading width
    • Comfortable reading width
    • Expanded reading width
  • Card for each section
  • Card with all content

 

USER'S GUIDE

LM2738 Step-Down Converter Evaluation Module User's Guide

Trademarks

All trademarks are the property of their respective owners.

1 Introduction

The LM2738 demo board is configured to convert 12-V input to 3.3-V output at 1.5-A load current using the LM2738X 1.6-MHz or the LM2738Y 550-kHz step down DC-DC regulator. The tiny low profile MSOP-PowerPAD-8 and WSON-8 packages allows the demo board to be manufactured using just over one square inch of a 4-layer printed circuit board.

The circuit is configured with the boost diode connected to VOUT, and according to the data sheet, VOUT must not exceed the maximum operating limit of 5.5 V + VfD2 using this configuration. This makes sure that the voltage between the boost and SW pins, VBOOST–VSW, does not exceed 5.5 V for proper operation. Please see the LM2738 550kHz/1.6MHz 1.5A Step-Down DC-DC Switching Regulator data sheet for more information regarding this requirement.

A bill of materials describes the parts used on this demo board. A schematic and layout have also been included along with measured performance characteristics. The schematics at the end of this document show how to re-configure this demo board for various input and output conditions as discussed in the LM2738 550kHz/1.6MHz 1.5A Step-Down DC-DC Switching Regulator data sheet. Short or leave open the indicated connection as indicated in the schematics. The above restrictions for the input voltage are valid only for the demo board as shipped with the demo board schematic (see Figure 2-1).

2 Operating Conditions

  • VIN = 12 V
  • VO = 3.3 V
  • IO = 1.5 A
GUID-F0BE49FC-C89B-4A27-8348-35F83E5E48B0-low.png Figure 2-1 LM2738 Demo Board Schematic - VBOOST Derived from VOUT = 3.3 V, VIN = 12 V
GUID-96911EF6-350B-4F2F-B81A-1455F410E20D-low.png Figure 2-2 Efficiency vs Load Current - VIN = 12 V, VOUT = 3.3 V
Table 2-1 Bill of Materials X-Version (1.6 MHz)
Part ID Part Value Manufacturer Part Number Package Type
C1, Input Cap 10 µF, 25 V, X7R TDK C3216X5R1E106 1206
C2, C5, Output Cap 22 µF, 10 V, X5R TDK C3216X5R1A226 1206
C3 (Boost Cap), C4 0.1 µF TDK C2012X7R1A104 0805
D2, Boost Diode 1 VF at 100-mA Diode Diodes, Inc. BAT54WS-TP SOD-323
R2, R3 10 kΩ, 1% Vishay CRCW12061002F 0805
U1 1.5-A Buck Regulator Texas Instruments LM2738 WSON-8
LM2738 MSOP-PowerPAD-8
D1, Catch Diode 0.34-VF Schottky, 1.5 A, 30 VR Toshiba CRS08 -
L1 5.0 µH, 2.9 A Coilcraft MSS7341-502NL -
R1 31.6 kΩ, 1% Vishay CRCW12063162F 0805
R5 0 Ω Vishay CRCW12060R00F 0805
D4, R4 Open or No Load
Table 2-2 Bill of Materials Y-Version (550 kHz)
Part ID Part Value Manufacturer Part Number Package Type
C1, Input Cap 10 µF, 25 V, X7R TDK C3216X5R1E106 1206
C2, C5, Output Cap 22 µF, 10 V, X5R TDK C3216X5R1A226 1206
C3 (Boost Cap), C4 0.1 µF TDK C2012X7R1A104 0805
D2, Boost Diode 1 VF at 100 mA Diode Diodes, Inc. BAT54WS-TP SOD-323
R2, R3 10 kΩ, 1% Vishay CRCW12061002F 0805
U1 1.5-A Buck Regulator Texas Instruments LM2738 WSON-8
LM2738 MSOP-PowerPAD-8
D1, Catch Diode 0.34 VF Schottky, 1.5 A, 30 VR Toshiba CRS08 -
L1 10.0 µH, 2.0 A Coilcraft MSS7341-103NL -
R1 31.6 kΩ, 1% Vishay CRCW12063162F 0805
R5 0 Ω Vishay CRCW12060R00F 0805
D4, R4 Open or No Load

 

Texas Instruments

© Copyright 1995-2025 Texas Instruments Incorporated. All rights reserved.
Submit documentation feedback | IMPORTANT NOTICE | Trademarks | Privacy policy | Cookie policy | Terms of use | Terms of sale