SPNU633 January 2020 RM42L432 , RM44L520 , RM44L920 , RM46L430 , RM46L440 , RM46L450 , RM46L830 , RM46L840 , RM46L850 , RM46L852 , RM48L530 , RM48L540 , RM48L730 , RM48L740 , RM48L940 , RM48L950 , RM48L952 , RM57L843 , TMS570LC4357 , TMS570LC4357-EP , TMS570LC4357-SEP , TMS570LS0332 , TMS570LS0432 , TMS570LS0714 , TMS570LS0714-S , TMS570LS0914 , TMS570LS1114 , TMS570LS1115 , TMS570LS1224 , TMS570LS1225 , TMS570LS1227 , TMS570LS2124 , TMS570LS2125 , TMS570LS2134 , TMS570LS2135 , TMS570LS3134 , TMS570LS3135 , TMS570LS3137 , TMS570LS3137-EP
Hercules, Code Composer Studio are registered trademarks of Texas Instruments.
Microsoft Office is a registered trademark of Microsoft Corporation in the United States and/or other countries, or both.
Windows is a registered trademark of Microsoft Corporation in the United States and/or other countries, or both.
All other trademarks are the property of their respective owners.
The HALCoGen compliance support package (CSP) was developed to provide documentation, reports and unit test capability to assist customers using HALCoGen generated software to comply with functional safety standards such as IEC 61508 and ISO 26262.
The HALCoGen Test Automation Unit (HALCoGen TAU) is a tool that helps users generate a Dynamic Coverage Analysis Report and Regression Report for HALCoGen generated drivers to support ISO26262 and IEC61508 assessments.
HALCoGen TAU comes with the unit test cases and functional test case for all of the modules supported by HALCoGen for the Hercules™ family of devices and the necessary test infrastructure to run these test cases. HALCoGen TAU also provides infrastructure for Hercules customers to add their own test cases for specific used cases.
NOTE
LDRA Unit is not provided as a part of the CSP download. To re-run the unit tests using the included Test automation unit software, customers are required to purchase and install LDRA Unit software from LDRA (See Section 12.15)