Eddie Esparza
Remember when science fiction movies would have a scene showing a fully automated factory managed by artificial intelligence? Such factories exist now!
An autonomous factory relies on real-time communication between individual components such as motion controllers and robots, and this communication must happen in real time. For example, one delayed motion command to a robot controlled by a programmable logic controller (PLC) 100 feet away could result in a defective end product.
Advancements in real-time Ethernet-based communication protocols have solved this problem. These protocols enable a large network of devices inside the factory to communicate with each other in real time, while also providing enough bandwidth to send diagnostic and control data to the cloud.
There’s a catch, however; although many real-time Ethernet protocols facilitate this communication, they aren’t interoperable. The result is that equipment set up to communicate through one real-time Ethernet protocol cannot easily accept another piece of equipment speaking a different protocol – even though both are using an Ethernet connection. So two questions arise: Which protocol should your equipment support, and can you enable multiple protocols?
Watch our multiprotocol demo | |
![]() |
Learn how to connect a Sitara evaluation module to three common Industrial networks |
Three major industrial Ethernet protocols have captured the majority of the industrial market: Profinet, EtherNet/IP and EtherCAT. Picking one of these three is generally a safe bet, but there are benefits and drawbacks to both single and multiprotocol support in a traditional ASIC setup, as listed in Table 1.
Single protocol | Multiprotocol | |
---|---|---|
Benefits | One hardware design for all equipment using that protocol | Captures more market segments using different protocols |
Challenges with using multiple ASICs | Ability to access only one segment of the market |
|
It’s apparent that from a commercial perspective supporting multiple protocols is the right answer, but implementing a multiprotocol solution can become costly and problematic for everyone from engineering to procurement. Figure 1 shows the flow of a company supporting multiple protocols using various ASICs. You can see that there are multiple devices required to make communication modules for each Ethernet solution, resulting in more complexity when creating various stock-keeping units (SKUs).
This flow can deter many factory equipment manufacturers from enabling various protocols on their products. But today, it’s possible to connect to more than protocol one using a multiprotocol-enabled device like a Sitara processor. A Sitara processor such as the AMIC110 enables many protocols with a single design, overcoming the potential challenges of designing a multiprotocol environment. However, Sitara processors offer an alternative way to design factory equipment that supports a variety of industrial Ethernet protocols. The benefits of Sitara devices simplify the flow for creating various SKUs as shown in Figure 2.
The industrial communication subsystem integrated into each processor enables you to create a single hardware design for various SKUs. All you have to do is load a new image onto the processor to connect the board to a new network. This strategic approach can not only lower your system design costs, but can also deliver these advantages:
In this video, we’ve created a set of demonstrations to show how to connect to a Profinet, EtherNet/IP or EtherCAT network using a single Sitara AMIC110 industrial communications engine.
Download the software today and run the demos on our evaluation module.
The Sitara AMIC110 processor is an entry-level device that can enable high integration and simplify development and warehouse management flow at a low cost—only $4 USD per unit. Sitara processors enable support for Profinet Isochronous Real Time (IRT), Profinet RT, EtherNet/IP and EtherCAT, with a single industrial-grade solution that has passed conformance for each of these protocols.
TI PROVIDES TECHNICAL AND RELIABILITY DATA (INCLUDING DATASHEETS), DESIGN RESOURCES (INCLUDING REFERENCE DESIGNS), APPLICATION OR OTHER DESIGN ADVICE, WEB TOOLS, SAFETY INFORMATION, AND OTHER RESOURCES “AS IS” AND WITH ALL FAULTS, AND DISCLAIMS ALL WARRANTIES, EXPRESS AND IMPLIED, INCLUDING WITHOUT LIMITATION ANY IMPLIED WARRANTIES OF MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE OR NON-INFRINGEMENT OF THIRD PARTY INTELLECTUAL PROPERTY RIGHTS.
These resources are intended for skilled developers designing with TI products. You are solely responsible for (1) selecting the appropriate TI products for your application, (2) designing, validating and testing your application, and (3) ensuring your application meets applicable standards, and any other safety, security, or other requirements. These resources are subject to change without notice. TI grants you permission to use these resources only for development of an application that uses the TI products described in the resource. Other reproduction and display of these resources is prohibited. No license is granted to any other TI intellectual property right or to any third party intellectual property right. TI disclaims responsibility for, and you will fully indemnify TI and its representatives against, any claims, damages, costs, losses, and liabilities arising out of your use of these resources.
TI’s products are provided subject to TI’s Terms of Sale (www.ti.com/legal/termsofsale.html) or other applicable terms available either on ti.com or provided in conjunction with such TI products. TI’s provision of these resources does not expand or otherwise alter TI’s applicable warranties or warranty disclaimers for TI products.
Mailing Address: Texas Instruments, Post Office Box 655303, Dallas, Texas 75265
Copyright © 2023, Texas Instruments Incorporated