Ben Kasemsadeh
Customers often ask me, “What are the effects of placing magnets near the sensor of an inductance-to-digital converter (LDC) such as the LDC1612?” Immunity to DC magnetic fields is particularly important in safety-critical systems and in systems that must be tamperproof, such as home-security systems.
The short answer is that narrowband LC sensors are immune to DC magnetic fields. Yet you can easily see a change in sensor inductance by moving a magnet near the sensor.
There are indeed two ways in which a DC magnet can change an LDC sensor reading:
It is important to note that these are secondary effects; they are not directly caused by the DC magnetic field. Let’s look at this question in more detail.
LDC sensors are narrowband resonators. They are affected only by AC magnetic fields that are at the same frequency as the sensor. The higher the Q of the sensor, the narrower its band is, and the more resistant it is to out-of-band interference.
A DC magnetic field such as the one generated by a permanent magnet does not change the sensor-oscillation frequency, and therefore does not alter the measurement results of an LDC.
To investigate the immunity to DC magnetic fields, I used an extremely strong neodymium magnet, which is the strongest type of permanent magnet commercially available (see Figure 1). The magnet measures 40mm by 40mm by 20mm and is seriously strong: It has a pull force of 80kg!
I measured the DC magnetic field strength with a Gauss meter and obtained a reading of 335mT at a distance of 3mm, as shown in Figure 2.
The permanent magnetic field does not interfere with the measurement. However, the conductive material that the magnet is made of acts as a target itself.
To exclude the impact that the magnet’s conductivity has on the LDC, I added a 1.6mm-thick aluminum shield between the magnet and the probe of the Gauss meter. As Figure 3 shows, the aluminum sheet does not impact the magnet’s DC magnetic field.
Next, I set up an LDC1612 with a 29mm diameter coil on a printed circuit board (PCB). The coil is taken from the LDC reference coil PCB and has 35 turns per layer, two layers, and 0.15mm trace width and spacing). With a 330pF capacitor, the sensor oscillates at a frequency of 1MHz.
Adding the aluminum sheet ensures that the LDC is exposed to the magnetic flux of the magnet, but not to the conductive material that the magnet is made of. At the chosen sensor frequency of 1MHz, the skin depth of aluminum is 82µm. Therefore, a 1.6mm-thick sheet of aluminum represents more than 19 skin depths. Since >99.9999998% of the current already flows within the first six skin depths, a 19-skin-depths-thick aluminum sheet prevents the conductive material of the magnet from interfering with the AC magnetic field generated by the sensor.
I compared the response of the sensor PCB under two test conditions, as shown in Figure 4:
At each point, I recorded the inductance data as measured by the LDC and the DC magnetic field strength.
Without the aluminum sheet, the sensor-coil inductance increased by 45% when I moved the magnet from a 3mm distance to a 50mm magnet-sensor distance, as shown in Figure 5.
However, when the aluminum sheet is present, a change in inductance was not observable (<0.01% between 3mm and 50mm).
Over the same range, magnetic field strength decreased 93%, from 335mT to 21mT.
The measurements show that the narrowband architecture of the LDC can detect the conductive material from which a magnet is made, but it is immune to interference from its magnetic field. A thin sheet of metal is sufficient to provide shielding from undesired metal interference, but no provisions against DC magnetic fields are required.
TI PROVIDES TECHNICAL AND RELIABILITY DATA (INCLUDING DATASHEETS), DESIGN RESOURCES (INCLUDING REFERENCE DESIGNS), APPLICATION OR OTHER DESIGN ADVICE, WEB TOOLS, SAFETY INFORMATION, AND OTHER RESOURCES “AS IS” AND WITH ALL FAULTS, AND DISCLAIMS ALL WARRANTIES, EXPRESS AND IMPLIED, INCLUDING WITHOUT LIMITATION ANY IMPLIED WARRANTIES OF MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE OR NON-INFRINGEMENT OF THIRD PARTY INTELLECTUAL PROPERTY RIGHTS.
These resources are intended for skilled developers designing with TI products. You are solely responsible for (1) selecting the appropriate TI products for your application, (2) designing, validating and testing your application, and (3) ensuring your application meets applicable standards, and any other safety, security, or other requirements. These resources are subject to change without notice. TI grants you permission to use these resources only for development of an application that uses the TI products described in the resource. Other reproduction and display of these resources is prohibited. No license is granted to any other TI intellectual property right or to any third party intellectual property right. TI disclaims responsibility for, and you will fully indemnify TI and its representatives against, any claims, damages, costs, losses, and liabilities arising out of your use of these resources.
TI’s products are provided subject to TI’s Terms of Sale (www.ti.com/legal/termsofsale.html) or other applicable terms available either on ti.com or provided in conjunction with such TI products. TI’s provision of these resources does not expand or otherwise alter TI’s applicable warranties or warranty disclaimers for TI products.
Mailing Address: Texas Instruments, Post Office Box 655303, Dallas, Texas 75265
Copyright © 2023, Texas Instruments Incorporated