Robert Taylor
When I started at TI, one of the first power supplies that I worked on was a high-current two-phase buck power supply for a processor core. The current was 40A – pretty large at the time, and too high to implement in a single stage. Most power-supply designers look to multiphase applications to split up high-current rails into stages that are more manageable in terms of power dissipation and size. You can also apply the same principles to lower-current systems to greatly reduce the size, while maintaining the other benefits of multiphase converters.
To illustrate how the multiphase approach compares to conventional single-stage designs, let’s look at a power-supply design for DDR4 memory. The input voltage for this design is 12V +/-10% and the output supplies 1.2V at up to 6A. I’ll compare two TI Designs Low Power DDR Memory Power Supply Reference Designs , both available on the TI Designs website. One uses the TPS62180 in a two-phase configuration, while the other uses the TPS53513. Figure 1 shows the two boards tested.
The total size for the two-phase solution is 10mm by 15mm, while the single-phase solution is 30mm by 15mm. You could optimize the components for both solutions further to reduce the space, because the size is really driven by the magnetics. The two-phase solution uses two 2mm-by-1.2mm inductors, while the single-phase solution uses one 7mm-by-6.5mm inductor. The two smaller inductors take up much less volume and are lower in cost than the single inductor.
Clearly, you can reduce space by going to a multiphase approach. But what about the efficiency? Figure 2 compares both supplies.
Full-load efficiency for the two-phase solution comes in at just under 80%, while the single-phase solution is around 87%. So there is a penalty in efficiency for greatly shrinking the size.
One point not clear from the graph above is the light-load performance. The efficiency at 15mA for the two-phase supply is 50%, while for the single phase it is 35%. This represents a difference of 20mW of lost power. While the difference is small, in a portable application this can lead to longer battery life.
Power-supply designers are always pushed to make smaller, more efficient designs. By taking a two-phase approach, you can save significant space, but at the sacrifice of full load efficiency. If efficiency is still the most important factor, there are solutions for that as well.
Special thanks to Ryan Manack for helping with the two designs and testing.
TI PROVIDES TECHNICAL AND RELIABILITY DATA (INCLUDING DATASHEETS), DESIGN RESOURCES (INCLUDING REFERENCE DESIGNS), APPLICATION OR OTHER DESIGN ADVICE, WEB TOOLS, SAFETY INFORMATION, AND OTHER RESOURCES “AS IS” AND WITH ALL FAULTS, AND DISCLAIMS ALL WARRANTIES, EXPRESS AND IMPLIED, INCLUDING WITHOUT LIMITATION ANY IMPLIED WARRANTIES OF MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE OR NON-INFRINGEMENT OF THIRD PARTY INTELLECTUAL PROPERTY RIGHTS.
These resources are intended for skilled developers designing with TI products. You are solely responsible for (1) selecting the appropriate TI products for your application, (2) designing, validating and testing your application, and (3) ensuring your application meets applicable standards, and any other safety, security, or other requirements. These resources are subject to change without notice. TI grants you permission to use these resources only for development of an application that uses the TI products described in the resource. Other reproduction and display of these resources is prohibited. No license is granted to any other TI intellectual property right or to any third party intellectual property right. TI disclaims responsibility for, and you will fully indemnify TI and its representatives against, any claims, damages, costs, losses, and liabilities arising out of your use of these resources.
TI’s products are provided subject to TI’s Terms of Sale (www.ti.com/legal/termsofsale.html) or other applicable terms available either on ti.com or provided in conjunction with such TI products. TI’s provision of these resources does not expand or otherwise alter TI’s applicable warranties or warranty disclaimers for TI products.
Mailing Address: Texas Instruments, Post Office Box 655303, Dallas, Texas 75265
Copyright © 2023, Texas Instruments Incorporated