Mark Knapp
I am sure this has happened to many of you: One morning, the engineering manager comes to you and says, “we need to add Wi-Fi® capability to product ‘x’, but I don’t want the circuit in product ‘x’ changed in order to add the capability.” If the existing system already has a universal asynchronous receiver/transmitter (UART) connection to a host processor, Wi-Fi capability can easily be added.
TI has created a reference design for a UART to Wi-Fi Bridge with 24 VAC Power (TIDA-00375) that is targeted for use in building automation and HVAC systems. This design features a low-power SimpleLink™ Wi-Fi CC3200 wireless MCU to enable Internet connectivity. This design also includes a power supply section that can be used with 24 volt AC systems found in HVAC applications and thermostats. The design can be interfaced to systems with either 3.3 volt or 5 volt logic.
The TIDA-00375 reference design is presented as a wireless bridge. (See Figure 1) The software included in the design creates a connection between two TIDA-00375 boards using a Wi-Fi connection provided by an external access point. Bidirectional communication is provided. The UART communications between the existing system hardware nodes appear as if a cable is connected between the two UARTs.
While this method is documented in the reference design, it is by no means the only use for this hardware. If no existing network is available, one of the two TIDA-00375 boards can be configured as an access point and the other board can then be connected to this network. Communications between the end systems would again appear as if the two systems were connected by a cable. This is shown in Figure 2.
Figure 3 shows a third possibility. In this configuration, one TIDA-00375 board is connected to an access point that has Internet access. Communication from the existing system can be sent to a cloud location on the Internet for remote monitoring of data, data analysis or even system control.
In addition to the HVAC and thermostat applications, there are many other possible applications for this design in building automation and factory automation. So, next time you are tasked with connecting existing hardware to Wi-Fi, remember our wireless bridge designs and the SimpleLink Wi-Fi CC3200 platform can help make the process easier. Let us know how you will use this reference design.
TI PROVIDES TECHNICAL AND RELIABILITY DATA (INCLUDING DATASHEETS), DESIGN RESOURCES (INCLUDING REFERENCE DESIGNS), APPLICATION OR OTHER DESIGN ADVICE, WEB TOOLS, SAFETY INFORMATION, AND OTHER RESOURCES “AS IS” AND WITH ALL FAULTS, AND DISCLAIMS ALL WARRANTIES, EXPRESS AND IMPLIED, INCLUDING WITHOUT LIMITATION ANY IMPLIED WARRANTIES OF MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE OR NON-INFRINGEMENT OF THIRD PARTY INTELLECTUAL PROPERTY RIGHTS.
These resources are intended for skilled developers designing with TI products. You are solely responsible for (1) selecting the appropriate TI products for your application, (2) designing, validating and testing your application, and (3) ensuring your application meets applicable standards, and any other safety, security, or other requirements. These resources are subject to change without notice. TI grants you permission to use these resources only for development of an application that uses the TI products described in the resource. Other reproduction and display of these resources is prohibited. No license is granted to any other TI intellectual property right or to any third party intellectual property right. TI disclaims responsibility for, and you will fully indemnify TI and its representatives against, any claims, damages, costs, losses, and liabilities arising out of your use of these resources.
TI’s products are provided subject to TI’s Terms of Sale (www.ti.com/legal/termsofsale.html) or other applicable terms available either on ti.com or provided in conjunction with such TI products. TI’s provision of these resources does not expand or otherwise alter TI’s applicable warranties or warranty disclaimers for TI products.
Mailing Address: Texas Instruments, Post Office Box 655303, Dallas, Texas 75265
Copyright © 2023, Texas Instruments Incorporated