SSZTD46 August 2024 TCAN3403-Q1 , TCAN3404-Q1
Christen Atkinson
Vehicles are evolving to include more advanced features enhancing safety, comfort and convenience. More features require more complex electronics, which emphasize the importance of power efficiency. Power efficiency enables longer driving ranges and lowers operational costs, resulting in semiconductor manufacturers lowering the typical supply voltage of an electrical component such as a microcontroller (MCU) from 5V to 3.3V. In many automotive systems, you now only need a 5V power rail for the 5V Controller Area Network (CAN) transceiver, while all other components can use a 3.3V or lower supply rail derived from the 12V, 24V or 48V battery. CAN transceivers operating from the 3.3V power supply would eliminate the need for the 5V rail and facilitate seamless interfacing with the MCU.
For automotive CAN networks currently in production, the only transceivers available that pass electromagnetic compatibility (EMC) standards also require a 5V power supply. Figure 1 shows a simplified block diagram of a 5V CAN node where the CAN controller is integrated into the MCU. With a 3.3V CAN transceiver, it is possible to use the 3.3V power supply for both the MCU and transceiver therefore reducing the overall bill-of-materials cost and board space.
3.3V CAN transceivers have existed in the industrial market for decades. Designers face two challenges when transitioning them to the automotive market, however; how to interoperate with existing 5V CAN transceivers and how to pass strict automotive EMC requirements. In this article, I’ll explain how TI’s 3.3V CAN transceivers can help overcome these challenges.
5V CAN transceivers are the incumbent solution for CAN networks, so it is essential that 3.3V CAN transceivers are fully interoperable within existing networks and architectures. For Tier1 automotive suppliers, interoperability is especially important, because they typically do not own the design of the whole CAN network. These suppliers will not know if the portion of the CAN bus they are designing will connect to a 3.3V or 5V transceiver. Interoperability between 3.3V and 5V CAN mitigates this risk. If 5V and 3.3V CAN transceivers are fully interoperable, it is no longer necessary to change all of the nodes on the communication bus to 3.3V. Subsystem designers have the flexibility to decide whether a single node on the CAN bus would benefit from a 3.3V transceiver.
TI’s 3.3V CAN families have been successfully tested to International Organization for Standardization (ISO) 16845-2. The testing covers a homogeneous network of all 3.3V transceivers and a heterogeneous network where four out of 16 CAN nodes are the 3.3V transceiver and the remaining 12 CAN nodes are a mix of three other industry-accepted 5V CAN transceivers. TI’s automotive 3.3V TCAN3403-Q1 and TCAN3404-Q1 transceivers have successfully passed this interoperability testing.
EMC performance of CAN transceivers is measured through two parameters: emissions produced by the device itself and immunity from interference present in the system. The TCAN3404-Q1 and TCAN3403-Q1 are compliant with the International Electrotechnical Commission (IEC) 62228-3 standard for EMC performance.
Emissions are the release of electromagnetic energy. Ideally, low emissions ensure that normal operation will not affect the performance of other nearby components. Immunity is a device’s ability to function without error in the presence of interference, such as emissions from other nearby components. Testing performed by third-party testing houses are among the most stringent tests for automotive applications and characterize the emissions and immunity performance of CAN transceivers.
5V CAN transceivers became popular because commercially available devices influenced the creation of EMC standards, while 3.3V CAN transceivers have struggled to overcome the challenges of meeting pre-existing standards. With TCAN3404-Q1 and TCAN3403-Q1’s ability to pass EMC requirements in a homogenous or heterogeneous network, this barrier has been overcome.
The TCAN3403-Q1 and TCAN3404-Q1 can pass stringent automotive EMC requirements and are fully interoperable with 5V CAN transceivers. As 3.3V becomes the standard supply voltage for automotive components, 3.3V CAN transceivers enable design flexibility to reduce the number of power supplies in the system to save power and cost.
For more technical information about 3.3V CAN transceivers, check out the technical white paper, “Automotive-Qualified Electromagnetic Compliant 3.3V CAN FD Transceivers.”
All trademarks are the property of their respective owners.
TI PROVIDES TECHNICAL AND RELIABILITY DATA (INCLUDING DATASHEETS), DESIGN RESOURCES (INCLUDING REFERENCE DESIGNS), APPLICATION OR OTHER DESIGN ADVICE, WEB TOOLS, SAFETY INFORMATION, AND OTHER RESOURCES “AS IS” AND WITH ALL FAULTS, AND DISCLAIMS ALL WARRANTIES, EXPRESS AND IMPLIED, INCLUDING WITHOUT LIMITATION ANY IMPLIED WARRANTIES OF MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE OR NON-INFRINGEMENT OF THIRD PARTY INTELLECTUAL PROPERTY RIGHTS.
These resources are intended for skilled developers designing with TI products. You are solely responsible for (1) selecting the appropriate TI products for your application, (2) designing, validating and testing your application, and (3) ensuring your application meets applicable standards, and any other safety, security, or other requirements. These resources are subject to change without notice. TI grants you permission to use these resources only for development of an application that uses the TI products described in the resource. Other reproduction and display of these resources is prohibited. No license is granted to any other TI intellectual property right or to any third party intellectual property right. TI disclaims responsibility for, and you will fully indemnify TI and its representatives against, any claims, damages, costs, losses, and liabilities arising out of your use of these resources.
TI’s products are provided subject to TI’s Terms of Sale (www.ti.com/legal/termsofsale.html) or other applicable terms available either on ti.com or provided in conjunction with such TI products. TI’s provision of these resources does not expand or otherwise alter TI’s applicable warranties or warranty disclaimers for TI products.
Mailing Address: Texas Instruments, Post Office Box 655303, Dallas, Texas 75265
Copyright © 2024, Texas Instruments Incorporated