SWRA750 September 2022
This application note is a testing guide for WL18xx Bluetopia devices. PLT tests are used at the production line after designing the board with the Wilinkâ„¢8 device. This is to sanity check the board works properly and detects any major design issues and manufacturing defects.
Basic RF commands like continuous TX/RX are required as well as part of the Regulatory certification process.
The Connection-less RF tests modes are connection-less RF spectrum tests which uses a spectrum analyzer for verification.
The BT SIG RF Testmode is meant for connecting with a Bluetooth® tester where the Wilink8 device is controlled over the LMP (Link Management Protocol)
There are two ways of issuing these test commands to Wilink8 device
Useful Links: