WiLink8 is a trademark of Texas Instruments.
Android is a trademark of Google Inc.
Bluetooth are registered trademarks of Bluetooth SIG, Inc.
Wi-Fi is a registered trademark of Wi-Fi Alliance.
Linux is a registered trademark of Linux Foundation.
All trademarks are the property of their respective owners.
The WL1835MODCOM8B board is tested to comply with ETSI/R&TTE over temperatures from –20°C to 85°C.
This board should not be modified to operate in other frequency bands other than what they are designed for.
FCC Licensing Requirements for the Wi-Fi and Bluetooth Radio Module of the EVM:
For evaluation only; not FCC approved for resale. This kit is designed to allow:
Per TI’s Regulatory Compliance Information located in the WL1835ModCOMB8B User’s Guide’s “Evaluation Board/Kit/Module (EVM) Additional Terms,” this EVM cannot be used for production purposes and is explicitly restricted from end-product introduction.
Use of this EVM requires the developer to provide a minimum distance of at least 20 cm from the antenna to all persons in order to minimize risk of potential radiation hazards.
Do not leave the EVM powered when unattended.
The WL1835MODCOM8B device is a Wi-Fi® MIMO, Bluetooth, and Bluetooth Low Energy (BLE) module board with the TI WL18MODGB module. WL18MODGB is built-in TI WL1835 IEEE 802.11 b/g/n and Bluetooth 4.2 solutions (5.1 compliant) to provide the best Wi-Fi and Bluetooth coexistence interoperability and powersaving technologies from TI.