SimpleLink, Texas Instruments, BoosterPack, LaunchPad, Code Composer Studio are trademarks of Texas Instruments Incorporated.
Wi-Fi are registered trademarks of Wi-Fi Alliance.
Bluetooth is a registered trademark of Bluetooth SIG, Inc.
Microsoft is a registered trademark of Microsoft Corporation.
All trademarks are the property of their respective owners.
The SimpleLink™ MCU portfolio offers a single development environment that delivers flexible hardware, software, and tool options for customers developing wired and wireless applications. With an ultimate goal of 100 percent code reuse across host MCUs, Wi-Fi®, Bluetooth® low energy, Sub-1 GHz devices, and more, choose the MCU or connectivity standard that fits your design. A one-time investment with the SimpleLink software development kit (SDK) lets you reuse often, opening the door to create unlimited applications. For more information, visit www.ti.com/simplelink.
The main use of the Radio Tool is to serve as a control panel for direct access to the radio. The tool can be used for the radio frequency (RF) evaluation, and for certification purposes (such as FCC, ETSI, Telec, and so on). The tool is expected to work seamlessly on TI evaluation platforms: BoosterPack plus FTDI emulation board for CC31xx devices, and LaunchPad for CC32xx devices. If customers want to use the tool on their final platform, see Section 11. The I/O levels of these lines should be kept at VBAT level (the same voltage that powers the CC31xx and CC32xx devices).
For reference RF numbers, see the CC3120 SimpleLink™ Wi-Fi® Wireless Network Processor, Internet-of-Things Solution for MCU Applications Data Sheet and the CC3220 SimpleLink™ Wi-Fi® Wireless and Internet-of-Things Solution, a Single-Chip Wireless MCU Data Sheet.