This application brief details the design considerations of the discrete power design for the AC8025 (from AutoChips™) system-on-chip (SoC) power rails with a power-management IC (PMIC) design. The design uses the TPS6593-Q1 PMIC, TPS62875-Q1 synchronous buck converters, and TPS745-Q1 low-dropout (LDO) regulators. The original power source is the battery. Then the battery voltage is converted to regulate the 5V or 3.8V bus. The LM25149-Q1 converts the battery voltage to regulate the bus voltage. All components in this design are automotive-qualified.
The TPS6593-Q1 IC has five buck converters and four LDOs. This PMIC is non-volatile memory (NVM) programmable, meaning the default register values are set in the TI production line to the desired values for this platform without further need for the customer to change settings. The full orderable part number for this one-time-programmable (OTP) spin is TPS6593C4C8RWERQ1. See the Technical Reference Manual for the specific part number for more details on the OTP settings.
This power design is an example of how required rails for AC8025 can be powered with TI PMIC, synchronous buck converters, and LDOs. This power design is possible to customize and optimize based on the actual use case regarding the SoC variant, current requirements, used peripherals, and so forth.
Table 1 shows the power rails, load requirements, and power group.
Power Rail | Voltage (V) | Current (A) | Power Group |
---|---|---|---|
LPDDR4, LPDDX4 | 1.1 | 2 | 5 |
D1V1_DDR | 1.1 | 5 | |
IVI_D1V8 | 1.8 | 3.5 | 3 |
IVI_A1V8 | 1.8 | 3 | |
SFT_0V8 | 0.8 | 0.5 | 2 |
IVI_D3V3 | 3.3 | 3.5 | 4 |
IVI_A3V3 | 3.3 | 4 | |
VDDQ_0V6 | 0.6 | 0.3 | 6 |
SFT_1V8 | 1.8 | 0.15 | 3 |
SFT_3V3 | 3.3 | 0.15 | 4 |
RTC_0V8 | 0.8 | 0.15 | 2 |
RTC_1V8 | 1.8 | 0.15 | 3 |
VCORE_0V8 | 0.8 | — | 1 |
IVI_A0V8 | 0.8 | 1 | |
UFS_1V2 | 1.2 | 2 | 3 |
RTC_3V3 | 3.3 | 0.15 | 4 |
Figure 1 shows a block diagram with LM25149-Q1, TPS6593-Q1, TPS62875-Q1, TPS628502-Q1, and TPS784-Q1 devices powering the AC8025 SoC power rails.
The main features of this power design include the following:
Figure 2 shows an example power-up timing of the power rails and power group corresponding signals.
Figure 3 shows the LM25149-Q1 schematic with critical components. For layout guidance, see the corresponding device data sheet and EVM user guide.
Figure 4 shows the TPS6593-Q1 and the LDO TLV793P-Q1 for MCU power supply schematic with critical components. For layout guidance, see the corresponding device data sheet and EVM user guide. For LDO input and output capacitor values, see the data sheet recommendation.
Figure 5 shows the TPS62875-Q1 schematic with critical components. For layout guidance, see the corresponding device data sheet and EVM user guide.
Figure 6 shows the TPS628502-Q1 schematic with critical components. For layout guidance, see the corresponding device data sheet and EVM user guide.
Figure 7 shows the TPS784-Q1 schematic with critical components. For layout guidance, see the corresponding device data sheet and EVM user guide.
The design outlined in this application brief, using the LM25149-Q1, TPS6593-Q1, TPS62875-Q1, TPS628502-Q1, and TPS784-Q1 provides the power requirements for AutoChips AC8025 SoC while maintaining good efficiency. This design is compact due to the minimum number of external components. The I2C control allows for diagnostic testing and other control of the TPS6593-Q1 device.
AutoChips™ is a trademark of NavInfo Co., Ltd.
All trademarks are the property of their respective owners.