비디오 시리즈
TI를 통한 Wi-Fi 6 이해
Wi-Fi에 관한 이 비디오 시리즈를 통해 흥미로운 IoT 연결의 세계를 발견해보세요! 이 비디오 시리즈에서는 IoT 연결을 원활하고 효율적으로 만드는 데 Wi-Fi의 기본 역할을 살펴봅니다. 초창기부터 Wi-Fi 6의 최첨단 발전까지 Wi-Fi의 발전에 대해 알아보고 그 성공의 기반이 되는 아키텍처를 이해하세요. Wi-Fi가 에지 노드에서 뛰어난 방법을 살펴보고 모듈 및 RF 인증에 대해 알아보세요. 노련한 기술 애호가이든 호기심 많은 학습자이든 이 시리즈는 IoT 및 Wi-Fi의 세계를 소개합니다.
Wi-Fi의 발전
발표자
리소스
Hello. In this short video, I will be discussing the evolution of Wi-Fi standards and why these new standards were added. 802.11 X terminology was originated by the IEEE, which sets the standards, while Wi-Fi X terminology is originated by the Wi-Fi Alliance which runs industry interoperability tests.
Here, I will show the mapping between the equivalent terms. Beginning with the first standard, IEEE 802.11 was released in 1997 followed by 802.11b and a in 1999. 802.11g came out in 2003. Wi-Fi 4 was later released in 2009, and Wi-Fi 5 in 2013. The newest developments include Wi-Fi 6 and Wi-Fi 6E, released in 2019 and 2020 respectively.
With Wi-Fi having been in the market for over 20 years, there have been numerous enhancements over time. The first standard, IEEE 802.11, was created to operate in the 2.4ghz frequency band with a singular channel size and a maximum data rate of 2 megabits per second. The 2.4ghz band is shared by many other wireless standards and the modulation used limited data rates causing low throughput. With each standard released after, the physical layer standards were enhanced to improve speed, throughput, and efficiency.
Previous standards use SISO, or single input, single output, which posed issues with bandwidth interference and throughput. Wi-Fi 4's release focused on increasing throughput with its biggest enhancement MIMO, or multiple input, multiple output, which allows users to receive and transmit simultaneously through multiple antennas.
A 40mhz channel was also added, which provided an increase in data rate availability over a singular 20mhz channel. Wi-Fi 4 included a power save mode that was on a fixed schedule to reduce energy consumption.
Recently, IoT has become an extremely important technology as people begin to use more and more devices as everyday objects. With Wi-Fi 4, it became possible to connect all of these devices to the internet enabling faster and more efficient communication across the globe. Furthermore, the release of Wi-Fi 4 was a milestone for IoT use.
Wi-Fi 5 was built for performance and aimed at solving the network congestion issue on the 2.4ghz band by using a less congested frequency channel, the 5 gigahertz band. Wi-Fi 5 introduced MU-MIMO to increase throughput speeds even more. MU-MIMO, or multi-use multiple input, multiple output, allows multiple users to access a wireless network simultaneously without interruption. It also uses 80mhz channels, quadrupling throughput, and increasing the maximum data rate to almost 7 gigabits per second. However, Wi-Fi 5 was not designed for the industrial use and is mainly used in smartphones, laptops, tablets, et cetera, as the 5 gigahertz band doesn't allow signals to travel far distances.
While all previous standards prioritized increasing throughput speeds, Wi-Fi 6 places more emphasis on increasing efficiency and decreasing congestion in high density environments. The Wi-Fi 6 standard introduces OFDMA, which allows for multiple user access by subdividing a channel, like subdividing a single road into multiple lanes for use by different cars at the same time. It also implements bidirectional MU-MIMO compared to only downlink MU-MIMO offered in Wi-Fi 5.
BSS coloring is used to color code shared frequencies which allows access points to determine if simultaneous use of the spectrum is possible, thus increasing network efficiency and data transmission in highly dense environments. Wi-Fi 6 introduced target wake time, a power saving mechanism that is more efficient than Wi-Fi 4 standard, as it can detect user activity to determine when to sleep and wake.
Overall, the latest Wi-Fi 6 standard brings greater scalability, reduced interference, faster performance, and lower latency, leading Wi-Fi 6 to be the next dominant enterprise Wi-Fi standard. An extension of Wi-Fi 6, Wi-Fi 6E introduces the new 6 gigahertz frequency band, a band never used before in Wi-Fi, providing essentially no interference with other devices.
Wi-Fi 6E was also designed with the goal of making the 160mhz channel more commonplace. Wi-Fi 6E uses the full bandwidth and spectrum of 6 gigahertz aimed to improve applications like 4K and 8K streaming, VR gaming, AR technology, and can be a benefit in IoT as well.
In review, the release of Wi-Fi 4 showed a large advance in Wi-Fi capabilities which Wi-Fi 5 and Wi-Fi 6 both built upon. Wi-Fi 4 introduced the dual band, another channel size, significantly higher speeds, and MIMO. Wi-Fi 5 introduced even more channel sizes, higher speeds, and MU-MIMO.
Wi-Fi 6 focuses on high efficiency and dense environments using more channel sizes for faster data rates. Wi-Fi 6 also introduced OFDMA, as well as other performance enhancing mechanisms. Wi-Fi 6E introduces the new 6 gigahertz band to reduce congestion. With the release of each of the newer Wi-Fi standards came an increase in the number of possible simultaneous spatial streams, allowing for the exponential increase in Wi-Fi users.
Wi-Fi standards have evolved greatly over the past 20 years, resulting in faster speeds and network efficiency for users around the world. There are many factors to consider when choosing a Wi-Fi standard and we hope that you can now effectively choose the right one for your system. If not, TI engineers are here to help you choose. For more information, please visit ti.com/wifi.