The license renews automatically every 30 days as long as you are connected to the internet. If you ever get an error about license expiration, simply connect to the internet and you should be able to continue using PSpice for TI.
The license renews automatically every 30 days as long as you are connected to the internet. If you ever get an error about license expiration, simply connect to the internet and you should be able to continue using PSpice for TI.
Yes. Each myTI login may get 1 license which is good for installations on up to 3 computers.
If you have installed PSpice for TI on less than 3 computers, you can install on an additional machine without issue. If you are already using your license on 3 machines and need to migrate your license from an existing machine to a new one, please click…
Your license validation about to expire. You must connect to the internet while using PSpice for TI at least once every 30 days. Please connect to the internet if you are not already online. When you launch PSpice for TI, the licenses will automatically…
Please check if you are connected to Internet. It could be that you had stayed offline for more than 30 days and the license needs to be validated. If you continue to receive this message, you may need to renew your license by logging in on TI.com. If…
Yes. PSpice for TI does need a license to run. This is installed as part of the software installation and it is validated periodically by the PSpice of TI application.
You can stay offline for 30 days. A license validation is required at least once every 30 days. The license validation occurs when you launch the tool and will need an internet connection. If you are still not connected to Internet after 30 days, PSpice…
Yes. PSpice for TI will need to connect over the Internet to validate your credentials the first time you launch the tool. If you planning to go offline after installation, we strongly recommend you stay connected the first few times using the tool before…
Try to re-install the PSpice for TI tool. See if you have internet connection. If you have valid internet connection and installation fails, please click here to open a new thread on the PSpice for TI E2E forum.
The error within the PSpice for TI tool means you have already used the Access Key to install on three separate machines which is the maximum. If you need to install on the new machine, please click here to open a new thread on the PSpice for TI E2E f…
Yes. The Installer will need to connect over the internet to download the PSpice® for TI software. Please ensure you stay online through the entire duration of the installation.
Your download link for PSpice® for TI will be valid for 30-days. If it is not used within 30 days, you need to register for access to the PSpice for TI tool again.
Yes. The same Access Key can be used to install PSpice® for TI on up to three machines.
Do you see the following: “Error displayed: Access key entered is not in expected format”.
Please verify if you have entered the Access Key as received in the email, including hyphens, and it should be in the following format -
Example:…
The Access Key for PSpice® for TI expires after one year. At that time, you will need to renew your registration. You can renew your registration by logging into ti.com. Then make a new request to download PSpice for TI.
The access key allows the user to install PSpice® for TI software and it is also checked by the PSpice for TI application while it is running.
If you lose your access key, you can register again on ti.com. A new email and download link will be provided, along with your existing access key. If that does not work, please click here to open a new thread on the PSpice for TI E2E forum.