SFRA

powerSUITE Digital Power Supply Software Frequency Response Analyzer Tool for C2000™ MCUs

SFRA

Overview

The Software Frequency Response Analyzer (SFRA) is one of several tools included in the powerSUITE Digital Power Supply Design Software Tools for C2000™ Microcontrollers.  The SFRA includes a software library that enables developers to quickly measure the frequency response of their digital power converter.  The SFRA library contains software functions that inject a frequency into the control loop and measure the response of the system using the C2000 MCUs’ on-chip analog to digital converter (ADC).  This process provides the plant frequency response characteristics and the open loop gain frequency response of the closed loop system.  The user can then view the plant and open loop gain frequency response on a PC-based GUI.  All of the frequency response data is exported into a CSV file, or optionally an Excel spreadsheet, which can then be used to design the compensation loop using the Compensation Designer

Maintained version of the library is available in the C2000Ware-DigitalPower-SDK. To get started using the SFRA in your own design, refer to “Chapter 2: Installing the SFRA Library” of the User’s Guide.

Older version with floating point support is available in controlSUITE , see User’s Guide.

The Software Frequency Response Analyzer GUI can be invoked in two ways:

  1. Launch Standalone:
    • Download C2000Ware-DigitalPower-SDK
    • Navigate to SFRA library directory inside the SDK and browse to the “gui” folder. Click on the Software Frequency Response Analyzer GUI icon to launch.
    • To understand how the Software Frequency Response Analyzer and the Compensation Designer work together, a case study is outlined in “Case Study” Chapter of the User’s Guide.
  2. Launch from the Solution Adapter inside powerSUITE:
    • Follow the steps on the Solution Adapter tool page.
    • Double click on the Software Frequency Response Analyzer icon from within the final step of the configuration process.
    • Click ‘Start Sweep’ to measure the frequency response of the digital power design.
For details on how to use the SFRA with an existing TI development kit, you can refer to the user guide for the development kit and browse to the "Customize Solution Using powerSUITE" section.
Features
  • Easy-to-use software library functions for measuring system frequency response
  • PC-based GUI for viewing Bode plots of power supply control loops

 

 

 

  • The Software Frequency Response Analyzer is included as part of powerSUITE
  • Software Frequency Response Analyzer (SFRA) Library Software
  • Software Frequency Response Analyzer (SFRA) Library User’s Guide
  • PC-based GUI for displaying Bode plots
  • Software code example of the SFRA software test bench

Download View video with transcript Video

Hardware development

DAUGHTER CARD
BOOSTXL-BUCKCONV Digital Power Buck Converter BoosterPack

Software development

DRIVER OR LIBRARY
CONTROLSUITE controlSUITE™ Software Suite: Software and Development Tools for C2000™ Microcontrollers
IDE, CONFIGURATION, COMPILER OR DEBUGGER
COMPENSATION_DESIGNER powerSUITE Digital Power Supply Compensation Designer Tool for C2000™ MCUs POWERSUITE powerSUITE - Digital Power Supply Design Software Tools for C2000™ MCUs SOLUTION_ADAPTER powerSUITE Digital Power Supply Solution Adapter Tool for C2000™ MCUs
SOFTWARE DEVELOPMENT KIT (SDK)
C2000WARE-DIGITALPOWER-SDK DigitalPower software development kit (SDK) for C2000™ MCUs

Support & training

TI E2E™ forums with technical support from TI engineers

View all forum topics

Content is provided "as is" by TI and community contributors and does not constitute TI specifications. See terms of use.

If you have questions about quality, packaging or ordering TI products, see TI support.

Videos