Get started on CC330x with Linux OS
Select a platform
BP-CC3301 — SimpleLink™ CC3301 Wi-Fi 6 and Bluetooth® Low Energy BoosterPack™ plug-in module
BEAGL-BONE-BLACK — BeagleBone® Black, community-supported development platform based on Sitara™ AM335x ARM® Cortex®-A8 Processor
BP-CC3301 — SimpleLink™ CC3301 Wi-Fi 6 and Bluetooth® Low Energy BoosterPack™ plug-in module
SK-AM62B-P1 — AM62x Starter Kit EVM with PMIC
BP-CC33-BBB-ADAPT — BP-CC33xx interface adapter for BeagleBone Black development platform
CC33XX-LINUX-MPU — CC33xx device driver source for MPUs running Linux OS.
CC33XX-LINUX-MPU — CC33xx device driver source for MPUs running Linux OS.
CC33xx Linux MPU Windows Installer
CC33xx Linux MPU Linux Installer
CC33xx Linux MPU Version 1.0.0.8 Logger Bin file
Products
Wi-Fi products
Hardware development
Evaluation board
Release Infomation
The CC33xx Linux MPU Software Package delivers components that enable engineers to develop connected applications on Texas Instruments Wi-Fi Companion-IC devices. The product is comprised of multiple software components and examples of how to use these components together. In addition, examples are provided to demonstrate the use of each functional area and each supported device and as a starting point for your own projects.
This CC33xx Linux MPU Software Package delivers components that enable operation of the Texas Instruments CC33xx Wi-Fi and BLE family of wireless transceivers on Linux platforms.
This is version **1.0.0.8** of the CC33xx Linux MPU Software Package
The version is a production quality release for 2.4/5Ghz devices
Previous release was 1.0.0.7
What's new
- Added new INI parameter to control TxPsatCompensation (0dB, 0.5dB, 1dB) - no change to default behavior
- Added new INI parameter to control RX AMPDU length: MaxRxAmpduLen (8K, 16K) - no change to default behavior
- Update in INI file the default setting of 'PowerSaveScheme' to 'no ps poll' mode - move to active for every TX \ RX
SIMPLELINK-WIFI-TOOLBOX — SimpleLink Wi-Fi Toolbox collection of tools to help development and testing of the CC33xx
SIMPLELINK-WIFI-TOOLBOX — SimpleLink Wi-Fi Toolbox collection of tools to help development and testing of the CC33xx
SimpleLink WiFi ToolBox Linux Installer
SimpleLink WiFi ToolBox Windows Installer
SimpleLink WiFi ToolBox MacOS Installer
SimpleLink WiFi ToolBox Intel MacOS Installer
Products
Wi-Fi products
Hardware development
Evaluation board
Documentation
Manifest
Release Infomation
SimpleLink Wi-Fi Toolbox is a cross-platform software kit, that provides all required tools for fast and easy ramp-up of the CC33xx family of devices. One of the included tools is Radio Tool.
Radio Tool is a tool for RF evaluation and testing of CC33xx designs, during development and certification. The tool enables low-level radio testing capabilities by manually setting the radio into transmit or receive modes. Usage of the tool requires familiarity and knowledge of radio circuit theory and radio test methods.
What's new
- Support Radio Tool for Wi-Fi 2.4GHz / 5GHz
- Support Radio Tool for BLE
- Support INI Composer
- Support Logging