ENERGYTRACE

EnergyTrace-Technologie

ENERGYTRACE

Downloads

Überblick

EnergyTrace™ software for MSP430™ MCUs, MSP432™ MCUs, CC13xx wireless MCUs and CC26xx wireless MCUs is an energy-based code analysis tool that measures and displays the energy profile of an application and helps optimize it for ultra-low-power consumption.

As most developers know, it is difficult to tune a system without understanding the state of the system. EnergyTrace software gives you the information needed to help you achieve the lowest power design. This feedback makes it easier to implement the various techniques offered by the MSP architecture, as well as the many tools provided by TI, such as the ULP Advisor.

This technology implements a new method for measuring MCU current consumption. Power is traditionally measured by amplifying the signal of interest and measuring the current consumption and voltage drop over a shunt resistor at discrete times. In debuggers that support EnergyTrace sofware, a software-controlled DC-DC converter generates the target power supply. The time density of the DC/DC converter charge pulses equals the energy consumption of the target microcontroller. A built-in calibration circuit in the debug tool defines the energy equivalent for a single charge pulse. Because the width of each charge pulse remains constant, the debugger can just count each charge pulse and then sum them over time to calculate an average current which leads to very accurate measurements. Using this approach, even the shortest device activity that consumes energy contributes to the overall recorded energy.

Another dimension of this software is called either:

  • EnergyTrace+ technology, also known as EnergyTrace+[CPU States]
  • EnergyTrace++ technology, also known as EnergyTrace+[CPU States]+[Peripheral States]

These modes take EnergyTrace to the next level. When debugging with devices that contain EnergyTrace+ or EnergyTrace++ support, you are presented with information about the internal states of the microcontroller in addition to the energy consumption of the system.

  • The CPU states include whether the device is in active mode or one of the many low-power modes (LPM).
  • The peripheral states show the ON-OFF status of the peripherals and all system clocks (regardless of the clock source).

With this tool, you can directly verify whether an application is running as expected. For example, you can make sure that a peripheral is turned off after a certain activity or system event.

Software & hardware requirements:

EnergyTrace software is included in Code Composer Studio™ IDE version 6.0 and later, as well as the latest version of IAR Embedded Workbench. It requires specialized debugger circuitry, which is supported with the MSP-FET or XDS110 emulators, as well as the emulators found on many of the MSP LaunchPad™ development kits.

EnergyTrace+ and EnergyTrace++ technology require additional circuitry within the silicon; therefore, these modes are only supported on select devices. The MSP432P4x family includes EnergyTrace+ features. The MSP430FR5x, MSP430FR6x, CC13x2 and CC26x2 MCUs contain the superset of EnergyTrace++ circuitry.

The following table summarizes what is supported with the different EnergyTrace™ software:

Features and devicesEnergyTrace™ softwareEnergyTrace+ softwareEnergyTrace++ software
Current monitoringxxx
CPU state (PC) xx
Peripheral or system state  x
Devices supportedAll MCUsAll MSP432P MCUs 

MSP430FR59xx/69xx

CC13x0/CC2640R2F

CC13x2/CC26x2

Compatible development toolsMSP-FET

TMDSEMU110-U (XDS110 Standalone)

TMDSEMU110-HDR (XDS110 Add-on)


eZ-FET with EnergyTrace

MSP-EXP430FR2311
MSP-EXP430FR2433
MSP-EXP430FR4133
MSP-EXP430FR5969
MSP-EXP430FR5994
MSP-EXP430FR6989

 

Embedded XDS110

MSP-EXP432P401R
MSP-EXP432P4111
LAUNCHXL-CC1312R1
LAUNCHXL-CC1352R1
LAUNCHXL-CC1352P1
LAUNCHXL-CC1352P-2
LAUNCHXL-CC1352P-4
LAUNCHXL-CC26XR1
LP-CC2652RB
MSP-FET + Adapter (MSP-FET-432ADPTR)

TMDSEMU110-U (XDS110 Standalone)

TMDSEMU110-HDR (XDS110 Add-on)

Embedded XDS110

MSP-EXP432P401R
MSP-EXP432P4111

MSP-FET

TMDSEMU110-U (XDS110 Standalone)

TMDSEMU110-HDR (XDS110 Add-on)

eZ-FET with EnergyTrace++

MSP-EXP430FR5969
MSP-EXP430FR5994
MSP-EXP430FR6989

Embedded XDS110

LAUNCHXL-CC1312R1
LAUNCHXL-CC1352R1
LAUNCHXL-CC1352P1
LAUNCHXL-CC1352P-2
LAUNCHXL-CC1352P-4
LAUNCHXL-CC26XR1
LP-CC2652RB

 

For a user guide to EnergyTrace software, refer to the chapters on EnergyTrace software in either the User’s Guide for Code Composer Studio™ IDE for MSP430™ MCUs, or the User’s Guide for Code Composer Studio™ IDE for SimpleLink™ MSP432 Microcontrollers. Or IAR Embedded Workbench™ IDE for MSP430 MCUs, or the IAR Embedded Workbench for Arm for for SimpleLink™ MSP432 Microcontrollers.

Merkmale
  • Current measurement is enabled for all MSP430 MCUs, MSP432 MCUs and connectivity devices
  • Tracing of CPU states is available on selected MSP430 MCUs, MSP432 MCUs, CC13x2 wireless MCUs and CC26x2 wireless MCUs 
  • Tracing of peripheral states is also available on selected MSP430 MCUs, CC13x2 wireless MCUs and CC26x2 wireless MCUs 
  • MSP430 MCUs require eZ-FET or MSP-FET debuggers in order to support EnergyTrace features
  • MSP432 MCUs require either the XDS110-ET (found on the MSP432 LaunchPad development kit) or the MSP-FET with the adapter for the MSP432 MCU
  • CC13x2 and CC26x2 devices require either the XDS110-HDR (found on the LaunchPad development kits) or the standalone XDS110 (TMDSEMU110-U) + EnergyTrace HDR accessory (TMDSEMU110-ETH)
  • Integrated into Code Composer Studio IDE and IAR Embedded Workbench (EW430 and EWARM)
Herunterladen Video mit Transkript ansehen Video

Downloads

IDE, Konfiguration, Compiler oder Debugger

ENERGYTRACE MSP EnergyTrace technology (delivered in Code Composer Studio™ IDE)

ENERGYTRACE MSP EnergyTrace technology (delivered in Code Composer Studio™ IDE)

close
Aktuelle Version
Version: null
Veröffentlichungsdatum:

Technische Dokumentation

Keine Ergebnisse gefunden. Bitte geben Sie einen anderen Begriff ein und versuchen Sie es erneut.
Alle anzeigen 14
Typ Titel Neueste englische Version herunterladen Datum
Technischer Artikel Pack a punch in battery pack systems with low-cost MCUs PDF | HTML 16.11.2021
Benutzerhandbuch Code Composer Studio IDE v10.x for MSP430 MCUs (Rev. AS) 05.05.2020
Technischer Artikel Visualizing the performance of the low-energy accelerator PDF | HTML 16.10.2017
Technischer Artikel Step 6 to build a smart thermostat using an MCU: energy optimization PDF | HTML 01.08.2017
Technischer Artikel How to create your own low-power telemetry logger for a drone PDF | HTML 25.07.2017
Technischer Artikel Celebrating #MSP430love PDF | HTML 13.02.2017
Technischer Artikel How to get more processing without sacrificing power consumption PDF | HTML 08.02.2017
Technischer Artikel Design a battery-powered building automation system to last for decades PDF | HTML 31.08.2015
Technischer Artikel The exclusive MSP back-to-school sale is here! PDF | HTML 26.08.2015
Technischer Artikel How FRAM can help you find your car PDF | HTML 23.07.2015
Technischer Artikel What is Compute Through Power Loss? PDF | HTML 29.05.2015
Technischer Artikel New LaunchPad - More Features - Big Savings PDF | HTML 22.05.2015
Anwendungshinweis Getting Started With EEMBC ULPBench on MSP-EXP430FR5969 (Rev. A) PDF | HTML 29.01.2015
Anwendungshinweis MSP430 Advanced Power Optimizations: ULP Advisor SW and EnergyTrace Technology 09.06.2014

Verwandte Designressourcen

Hardware-Entwicklung

Entwicklungskit
LAUNCHXL-CC1312R1 CC1312R LaunchPad™ development kit for sub-1-GHz SimpleLink™ wireless MCU LAUNCHXL-CC1352R1 CC1352R LaunchPad™ development kit for SimpleLink™ multi-band wireless MCU LP-CC1311P3 CC1311P3-LaunchPad™ Entwicklungskit für SimpleLink™ drahtlose Sub-1-GHz-MCU MSP-EXP430FR2311 MSP430FR2311 LaunchPad™ development kit MSP-EXP430FR2433 LaunchPad™-Entwicklungskit MSP430FR2433 MSP-EXP430FR4133 LaunchPad™-Entwicklungskit MSP430FR4133 MSP-EXP430FR5969 MSP430FR5969 LaunchPad™-Entwicklungskit MSP-EXP430FR5994 MSP430FR5994 LaunchPad™ development kit MSP-EXP430FR6989 MSP430FR6989 LaunchPad™ development kit
Evaluierungsplatine
LAUNCHXL-CC1352P CC1352P LaunchPad™-Development Kit für SimpleLink™ drahtlose Multi-Band-MCU LAUNCHXL-CC26X2R1 CC26x2R LaunchPad™ Development Kit für Multi-Standard SimpleLink™ Drahtlos-MCU
Hardware-Programmiertool
MSP-FET MSP MCU-Programmiermodul und -Debugger

Software-Entwicklung

IDE, Konfiguration, Compiler oder Debugger
CCSTUDIO Integrierte Entwicklungsumgebung (IDE) Code Composer Studio™

Support und Schulungen

TI E2E™-Foren mit technischem Support von TI-Ingenieuren

Alle Forenthemen anzeigen Alle Forenthemen auf Englisch anzeigen

Inhalte werden ohne Gewähr von TI und der Community bereitgestellt. Sie stellen keine Spezifikationen von TI dar. Siehe Nutzungsbedingungen.

Bei Fragen zu den Themen Qualität, Gehäuse oder Bestellung von TI-Produkten siehe TI-Support.

Videos