Seleccione una versión

Seleccione una versión

No se encontraron resultados. Borre su búsqueda y vuelva a intentarlo.

C29-CGT

C29 code generation tools -- compiler

Seleccione una versión
No se encontraron resultados. Borre su búsqueda y vuelva a intentarlo.
Última versión
Versión: 2.2.0.LTS
Fecha de publicación: 26/02/2026

Información de la versión

This is the 2.2.0.LTS Long-Term Support (LTS) release of the TI C29 Clang (c29clang) Compiler Tools. The c29clang compiler tools provide software development tools including the compiler, assembler, and linker, among others, which can be used to develop applications with C/C++ source code for loading and running on C29 core processors.

For definitions and explanations of STS, LTS, and the versioning number scheme, please see https://software-dl.ti.com/ccs/esd/documents/sdto_cgt_compiler_version_numbers_and_what_they_mean.html.

 

Novedades

  • Support for link-time optimization with -flto
  • The compiler tools now support linking -mfpu=f32 code into -mfpu=f64 projects. Previously, this resulted in a link-time error.
  • Security support in linker command files have been enhanced with more options. See the Compiler User's Guide chapter "The Safety and Security Unit" for details.
  • New floating point mode: -mfpu=none, which emulates all floating point operations in general-purpose registers. Used to avoid saves/restores of floating-point registers on-entry to an interrupt.
  • At -O3, integer division sequences are now emitted inline, rather than called
  • Memory operations will more intelligently use the built-in address scaling of offset registers
  • General reduction of superfluous or redundant sign and zero extension
  • More performant C-library math.h functions via the use of -ffast-math or through intrinsics. See the Compiler User's Guide chapter "Built-In Functions and Intrinsics" for details.