BQEVSW — bq Evaluation Software (bqEVSW) v0.0.92 for bq30z554-R1
サポート対象の製品とハードウェア
製品
バッテリ残量計
BQEVSW — bq Evaluation Software (bqEVSW) v0.0.92 for bq30z554-R1
bqEVSW 0.09.0092 windows installer
bq Evaluation software(bqEVSW) is a software tool to assist with the process of evaluating, designing with, configuring, testing, or otherwise utilizing the bq20xxx and bq30xxx series of TI Battery management products. It includes features that provide full access to registers and data memory including support for real-time logging, direct low-level communication, as well as support for configuration and calibration.
Note for EV2300: The EV2300 product page provides drivers for 32-bit windows. It may be possible to use 64 bit Windows 7 or newer 64 bit Windows with the unofficial 64 bit EV2300 driver posted on TI e2e forum.
** May require installation of EV2400 support components from EV2400 product page.
bqEVSW 0.09.0092 windows installer
SDK, API, and Programmer installer
Quick Tips text document for Command line programmers
Software Manifest
Description:
BQ-BATTERY-PROGRAMMER-SW software development kit (SDK) is a collection of robust software command line tools that assist with the process of programming, testing, or assembling packs that use TI Battery management products. The executables in this software work with the MKST-3P-ALT-EV2300 MKS Technology alternative for EV2300 communications transceiver. The executables work with a single station but can be extended to multiple stations by using additional software and GUI from MKS Technology Inc. . Support for multiple stations is not included in this software.
There are multiple executables in the download, usually one per family of products. Older products such as BQ20xxx and BQ30xxx are also supported. Examples using the C++ programming language API and Python® programming language are provided for custom development.
Requirements:
Features:
Getting started:
1. Download the software
2. Run the installer
3. The executables, C API and Python API files can be found in the install location
4. Run the command line executable without arguments to get usage help. Refer to Readme.txt in the install folder for more information and how to get help using the command line.
Software installer to enable BQEVSW to use MKST-3P-ALT-EV2300
Software manifest
Description:
BQEVSW-MKST-UPDATE software is a software update for BQEVSW (bq Evaluation Software) and BQEASY (bq EV-Easy) to allow it to work with the MKST-3P-ALT-EV2300 MKS Technology alternative for EV2300 communications transceiver. This update installs a program that allows switching the USB transceiver target in software like BQEVSW and BQEASY from/to EV2300 to/from MKST-3P-ALT-EV2300.
The program requires administrator privileges.
Requirements:
Features:
Getting started:
1. Download the software
2. Run the installer and check the option to create shortcuts
3. Run the program using shortcut named BQEVSW-MKST-UPDATE from Start menu/Desktop
4. Allow administrator privilege when/if prompted
5. On the GUI window that opens, select the target transceiver to support and follow steps to switch
6. Connect matching transceiver and start BQEVSW, BQEASY or other similar software.
Note: BQMTESTER-MKST-UPDATE and BQEVSW-MKST-UPDATE both update the same software components. Switching the USB transceiver using any of these shortcuts will also switch it in the other.
Important Note: The latest chemistry updater for bqStudio requires bqStudio 1.3.86 or higher. |
Instructions for bqStudio Chemistry database update:
Instructions for bqEVSW Chemistry database update: