Understanding the pitfalls of discrete level shifting circuits
Resources
Hello, my name is Atul Patel. I'm a product marketer on TI Standard Logic Team. In this brief video, I'll be reviewing some of the pitfalls of using discrete component base level shifting solutions, as well as introducing TI's new 2N7001T, a single-bit level-shifter device. The 2N7001T was designed to help system designers implement simple uni-directional level shifting solutions where historically discrete level-shifting implementations may have been used.
In today's complex systems with multiple operating voltage nodes, there is often a need to level shift I/O levels between devices that operate on different voltage nodes. The most common example is the communication between a processor and a peripheral device that operate on two different voltage nodes, such as 3.3 volt and 1.8 volt, as shown here. The level-shifting device in this example helps to shift the output of the processor up to meet the input requirements of the peripheral device. Conversely, down translation would be needed for the 3.3 volt to 1.84 volt direction. Simple uni-directional level shifting such as this plays a critical role in today's system in helping to interconnect core components of a system design.
To help address the market demand for simple uni-directional push/pull eye level shifting, Texas Instruments is introducing the 2N7001T, a single-bit uni-directional level shifter. The device was developed to help system designers implement simple uni-directional level-shifting solutions from 1.8 volt to 3.3 volt, where historically discrete level shifting implementations may have been used. The key advantages of using the 2N7001T instead of discrete components, like FETs and resistors, are smaller overall implementation size, reduced component count, simplified signal routing, and better overall signal performance without significantly impacting implementation cost.
Some of the key features of the device include 1.8 volt to 3.6 volt level shifting, operating voltage temperature range from minus 40 to 125 C, ESD protection up to 1 kV HBM and 500 volts CDM, 12 milliamps of output current drive, as well as VCC isolation, and partial power down functionality. Additional benefits such as lower power dissipation, sourcing fewer components, and lower board build cost can be achieved, depending on application-specific design objectives.
The device was developed for use in a wide variety of applications ranging from industrial applications to personal electronics, as well as automotive and communications. The device is available in two package options, including a standard SC-70 SOT package, as well as a much smaller X2SON microQFN package, enabling implementation in virtually any application.
In the layout example shown, a four FET discrete implementation is compared to the 2N7001T and the SC-70 or DCK package. As you can see, there's a substantial savings where the discrete solution takes up approximately 60 millimeters square of board space versus the integrated solution, about 10 millimeters square of board space. Overall, the 2N7001T is an ideal choice for applications needing simple uni-directional push/pull level-shifting solution.
Now let's take a quick look at how a common discrete push/pull level-shifting implementation compares with the 2N7001T. The discrete solutions, by their nature, are simple and have basic operational functionality with no specific level translation parameters that can be analyzed for understanding performance. The discrete level translation implementation shown in this example consists of four discrete components that provide simple level translation between a processor and peripheral device.
Some of the pitfalls or drawbacks to the discrete solution like this are larger solution size in terms of board space consumed by the components. In addition, adjusting data rate will require different pull up resistor values, making the implementation less suitable for dynamic applications. Discrete implementations also less power efficient, often forcing designers to make power versus data rate trade-offs. Designers also need to deal with glitches, and discrete solutions have no inherent VCC isolation.
Dedicated level shifter solutions such as the 2N7001T provide multiple benefits over discrete implementations. With a 2N7001T, a single component replaces multiple discretes, reducing board space and eliminating a complexity of connecting multiple devices. The 2N7001T also enables system designers to achieve higher data rates without sacrificing power, as well as much better signal performance.
The integrated nature of the device inherently provides VCC isolation, as well as better overall signal performance that results from deterministic rise and fall times, enabling much easier interfacing to downstream components. Overall, the 2N7001T versus a discrete solution provides a much more robust solution for implementing simple uni-directional push/pull level shifting applications.
Next, let's take a look at a comparison of common discrete implementations and their pitfalls. Since discrete solutions can be implemented using many different combinations of components, this table is meant to provide a comparison between different discrete implementations and an integrated solution such as the 2N7001T.
BJT-based solutions, although very simple, have multiple drawbacks, such as higher component count, higher leakage, as well as poor signal integrity, in addition to requiring power sequencing. Slightly more complex discrete solutions that use NMOS FETs provide marginally better signal performance than BJT solutions still suffer from higher leakage, limited data rate, and still require power sequencing.
Classic NMOS PMOS push/pull discrete implementations offer better signal performance in terms of rise and fall times compared to NMOS implementations. However, this type of discrete implementation still requires a trade-off between power and data rate, and often fails to provide VCC isolation as well as a glitch-free operation. In addition, discrete NMOS PMOS solutions could require power sequencing, as well as additional ESD protection components, further increasing implementation cost and complexity.
In contrast to discrete implementations, the 2N7001T allow system designers to use a single component to implement uni-directional level shifting function with the added benefits of smaller implementation size, lower leakage, VCC isolation, support for higher data rates, as well as built-in ESD protection, and worry-free power sequencing. Overall, the 2N7001T provides a much more robust solution than compared to these different discrete implementations of I/O level shifting and should be considered whenever implementing any sort of push/pull uni-directional level shifting solution.
For more information on the 2N7001T, please visit TI's product page at the link shown, or search for 2N7001T.
Thank you for your attention.
This video is part of a series
-
Logic and voltage translation
video-playlist (20 videos)