Internet Explorer is not a supported browser for TI.com. For the best experience, please use a different browser.
Video Player is loading.
Current Time 0:00
Duration 9:58
Loaded: 0.00%
Stream Type LIVE
Remaining Time 9:58
 
1x
  • Chapters
  • descriptions off, selected
  • en (Main), selected

[MUSIC PLAYING]

Hello and welcome to the TI Precision Labs series on current sense amplifiers. My name is Kyle Stone, and I am a product marketing engineer in the current and position sensing product line. In this video, we will introduce the most common sources of error in current sense amplifier circuits. Each error source will be explained further in later videos within this series.

There are several errors sources that can affect current sensing circuits. And they can be grouped together into three main categories. The first error type is offset error. Input offset voltage, VOS, common mode rejection ratio, CMRR, and power supply rejection ratio, PSRR, all create an offset voltage at the input of the device that remains mostly constant across the entire input range. In general, offset error is the dominant error type at low input levels.

The second error type is gain error. The gain error and linearity of the amplifier, coupled with the tolerance of the shunt resistor, all create errors that vary with input signal level. In general, gain error is the dominant error type at high input levels.

The third type of error is application-dependent error. This includes error induced by bias currents, temperature variations, input filters, frequency response limitations, and any other artifacts. As the name implies, the impact of this type of error can vary significantly across different types of applications and devices.

System designers often need to combine these error sources together to calculate the total error of the system and make sure it meets their requirements. There are two common ways to do this. First, the worst-case total error is calculated by simply summing the maximum possible errors together. This is a very conservative approach.

However, common statistical analysis tells us that these errors have distributions. And it is almost impossible to find a device with maximum error of each type. A more realistic approximation of total error can be determined by using the root sum of the squares, RSS method, to combine the error types. To use this method, take the square of the maximum value for each error source, add them together, then take the square root of the result.

Let's look at an example of offset error. This is an example of a refer to input or RTI specification. Something must be added to the input before the device gain. For this example, we'll consider an amplifier with a gain of 50 volts per volt and an input offset voltage of only 100 microvolts. The input voltage range VIN is from 0 volts to 100 millivolts.

To calculate VOUT ideal, the ideal output voltage of the amplifier with no errors whatsoever, we simply multiply the input voltage by the gain. This results in a range from 0 volts to 5 volts. To calculate VOUT actual, the actual output voltage, we must add the input offset voltage to the input voltage before multiplying by the gain. This results in a range of 5 millivolts to 5.005 volts. To calculate the percent error, the absolute value of VOUT actual minus VOUT ideal is divided by VOUT ideal.

Let's look at the results of this error calculation on the next slide. The plot on the left shows the output error in volts between the actual and ideal outputs, which is a constant 5 millivolts across the entire input range of 0 to 100 millivolts. Calculating the percent error gives us a much different result. The error becomes large at 0 input voltage since the error voltage of 5 millivolts is large compared to the ideal output of 0 volts.

The error dropped significantly with larger input levels, dropping to less than 1% at 10 millivolts of input signal. Designing for a specific operating region can help mitigate these offset errors. Maintaining an input voltage which is significantly larger than the input offset voltage reduces the effect of the input offset voltage on the measurement.

Let's now consider a similar example that illustrates gain error. We will ignore any offset error for simplicity. Here we will consider an amplifier with a gain of 200 volts per volt and a gain error of 3%. The input voltage range is still 0 to 100 millivolts.

Again, to calculate VOUT ideal, we will simply multiply the input voltage by the gain. This results in a range of 0 to 20 volts. To calculate VOUT actual, we will multiply the input by the nominal gain plus or minus the extra percentage of error. This results in a range of 0 to 20.6 volts. Percent error is calculated the same way as before.

Let's look at the results on the next slide. The plot on the left shows the output error in volts between the actual and the ideal outputs. In this case, you can see the error voltage change linearly with the input voltage. As you might expect, plotting the percent error gives a different result, in this case a constant 3% over the entire input range.

If we consider the effect of amplifier non-linearity as well, the error line would no longer be straight. Instead, it would look more like the blue curve, depending on the internal architecture of the amplifier. We recommend selecting an amplifier with a gain error specification that meets or exceeds your total error requirement.

Finally, let's consider some other types of error. Changes in temperature affect the performance of a current sense amplifier and all integrated circuits in general. Input offset voltage and gain error drift over temperature are usually specified in a product datasheet. PSRR and CMRR are not always given drift values, but minimum and maximum values are given both at room temperature and over the entire operating temperature range.

Shunt resistor value changes are specified by the resistor manufacturer, often called the temperature coefficient or tempco of the resistor. Input bias currents in a current sense amplifier are typically larger than in a traditional op amp, dif amp, or instrumentational amp. These biased currents are typically under 50 microamps. But depending on the system, they can cause issues at very low current levels with large resistors.

Finally, other application-specific factors like printed circuit board PCB layout, passive filtering at the device input, and other aspects of the device's internal architecture can contribute to the measurement in accuracies as well. Please remember that this video is only an introduction to each of these error sources.

The next videos in this series will give more detail on each error source and how to manage them in your designs to achieve high performance. That concludes this video. Thank you for watching. Please try the quiz to check your understanding of the content. For more information and videos on current sense amplifiers, please visit ti.com/currentsense.

This video is part of a series