Internet Explorer is not a supported browser for TI.com. For the best experience, please use a different browser.
Video Player is loading.
Current Time 0:00
Duration 1:39
Loaded: 10.02%
Stream Type LIVE
Remaining Time 1:39
 
1x
  • Chapters
  • descriptions off, selected
  • en (Main), selected

In this video, an example of a MOSFET circuit will be used to determine its output voltage characteristics using DC nested sweep in PSpice. First, create a new simulation profile for the circuit. Name the profile as "DC sweep," and click the Create button. The simulation settings GUI opens.

Under Analysis Type, choose DC Sweep from the dropdown list. DC sweep analysis in PSpice allows you to sweep a source, voltage, or current, a global parameter, a model parameter, or the temperature through a range of values.

For the example circuit, let's very drain-to-source voltage, VDS, from 0 to 10 volts with an increment of 100 millivolts. To create an nested sweep, click on the Secondary Sweep option and vary the DC input voltage source, VGS, from zero to five volts with an increment of 0.5 volts. Click OK to save the simulation settings.

Add a current marker on the drain terminal of the MOSFET. This will potentially plot a graph of drain-to-source voltage on the x-axis versus the drain current on the y-axis with varying gate-to-source voltage after simulation is performed. Click the icon to run the simulation.

The waveform displayed shows the different operating regions of the MOSFET, namely ohmic, saturation, and cut off region. It represents the output characteristic curves of the MOSFET. Now you can successfully perform a DC nested sweep analysis with PSpice.

This video is part of a series