Tiny Texas Instruments power circuit simplifies USB battery charger design
1.1-A single-cell Li-Ion battery charger with integrated 50-mA regulator
offers 2.3-A production test support, high-voltage protection
Bangalore (April 15, 2009) - Texas Instruments Incorporated (TI) introduced today the industry’s smallest 1.1-A Li-Ion linear battery charger with integrated 50-mA low-dropout regulator to support mobile phones and other handheld electronics. The new bq25040 comes in a small 2 mm x 3 mm package, and can regulate voltage within one-percent accuracy from a USB port or AC adapter. The device’s integrated LDO allows a mobile application to power up instantly from an external power source, even with an empty or absent battery. For details and samples see: www.ti.com/bq25040-pr .
The bq25040 also saves manufacturing time and cost by eliminating the need for battery setup during production test phase. The charger’s single-input interface selects the appropriate charge current and places the device into production test mode.
Key features and benefits
- 30-V input with overvoltage protection enables safe charging with unregulated or aftermarket adapters
- Up to 1.1-A charge rate
- Integrated 50-mA LDO supplies power to external circuits, such as a USB transceiver
- Production test mode regulates 4.2-V output without battery connection, and supplies up to 2.3 A
- Selectable 100-mA or 500-mA USB current limit complies with USB standard
- Input voltage dynamic power management provides protection against poor USB sources
Find out more about TI’s battery charge management portfolio:
About Texas Instruments:
Texas Instruments (NYSE: TXN) helps customers solve problems and develop new electronics that make the world smarter, healthier, safer, greener and more fun. A global semiconductor company, TI innovates through manufacturing, design and sales operations in more than 25 countries. For more information, go to www.ti.com.
Trademarks
All registered trademarks and other trademarks belong to their respective owners. |