Placement Silo Title

News Releases

Media Coverage

Media Kit

Texas Instruments introduces products in new PicoStar™ package, industry’s thinnest package for portable consumer electronics

Power management IC provides 65-µA quiescent current

Bangalore (May 8, 2009) - Portable consumer electronics designers can save board space with integrated circuits (ICs) in the PicoStar™ package that Texas Instruments Incorporated (TI) introduced today.  The ultra-thin package, about as thin as a human hair, is the first to give system designers the option to embed silicon components inside the printed circuit board (PCB) to maximize board space.  Devices in this form factor are 50 percent thinner than similar chips in traditional packages and enable smaller, thinner end equipment. The TPD2E007, a two-channel, robust electrostatic discharge (ESD) solution, is the first device available in the ultra-thin PicoStar package. For product details and to order samples see: www.ti.com/tpd2e007-pr.

The TPD2E007 is a back-to-back diode array that allows AC-coupled data transmission without compromising signal integrity. Typically, ESD protection is mounted close to the connector on the PCB, but designers have the option to surface mount or embed the TPD2E007 into the board/connector. The ability to embed this ultra-thin device in the board allows designers to save 80 percent board space compared to typical ESD solutions.

Key features of the TPD2E007

  • Robust ESD protection
    • ±8-kV IEC 61000-4-2 contact discharge
    • ±15-kV IEC 61000-4-2 air-gap discharge
  • Back-to-back diode configuration for negative signal swing
  • 15-pF line to ground capacitance
  • Low 50-nA leakage current
  • PicoStar package: 0.15 mm package height

Key benefits

  • Reduces board space, which gives end equipment designers the option to add more components on the board
  • Thin form factor allows the device to be inserted into a board layer stack-up with minimal effort
  • Board-level cost can be reduced by embedding the device in the PCB

Find out more about TI’s ESD protection portfolio by visiting the links below:

About Texas Instruments:

Texas Instruments (NYSE: TXN) helps customers solve problems and develop new electronics that make the world smarter, healthier, safer, greener and more fun.  A global semiconductor company, TI innovates through manufacturing, design and sales operations in more than 25 countries.  For more information, go to www.ti.com.

Trademarks

All registered trademarks and other trademarks belong to their respective owners.