Easy regulation compliance and improved energy efficiency made possible with TI’s new low-cost PiccoloTM MCU Motor Control Kits with PFC
Two new kits are industry's first to enable power factor correction and sensorless control of up to two motors using one MCU
Bangalore (June 29, 2009) — Power factor correction (PFC) is becoming a key requirement for motor control applications, as regulation standards aimed to prevent spikes in the power grid are increasingly implemented. Texas Instruments Incorporated (TI) announces two new Piccolo Motor Control Kits that enable PFC and sensorless field-oriented control of up to two motors with a single low-cost microcontroller (MCU). Leveraging TI’s Piccolo MCUs and high-performance analog, the kits include everything needed to immediately begin development of cost-sensitive motor control applications such as pumps, HVAC, refrigerators and other appliances/white goods. Allowing developers to efficiently meet their design needs, these controlCARD-based kits include a Piccolo controlCARD, Code Composer Studio™ IDE, software libraries and a hardware designer’s package. The Motor Control and PFC Developer’s Kit includes a single permanent magnet motor while the Dual Motor Control and PFC Developer’s Kit includes two. For more information, visit www.ti.com/1motorcontrolpfc-prtools or www.ti.com/2motorcontrolpfc-prtools.
Key features and benefits of the Piccolo MCU Motor Control and PFC Developer’s Kits
- Single 60MHz TMS320F28035 MCU features 128KB flash and control-oriented peripherals such as 12-bit, 16 channel on chip ADC and high resolution PWM outputs
- Sensorless field-oriented software tuned for kits’ motors allows developers to easily begin design right out of the box
- Software is broken into incremental builds for easy, step by step learning and development of motor control plus PFC on Piccolo MCUs
- Dual full bridge PWM motor drivers include programmable cycle-by-cycle current limit and two stage thermal protection capabilities
- Isolated onboard USB JTAG emulation saves on cost by eliminating the need for an external JTAG emulator
- Detailed documentation of field-oriented motor control theory and PFC principles, including instructions for executing both with one Piccolo MCU
Find out more by visiting the links below:
About Texas Instruments
Texas Instruments (NYSE: TXN) helps customers solve problems and develop new electronics that make the world smarter, healthier, safer, greener and more fun. A global semiconductor company, TI innovates through design, sales and manufacturing operations in more than 30 countries. For more information, go to www.ti.com.
Trademarks
All registered trademarks and other trademarks belong to their respective owners.
India Product Information Centre
Toll: +91-80-4138 1665
Toll free: +1-800-425-7888
Email: tiasia@ti.com
|