Texas Instruments simplifies system design and layout with industry’s first isolated CAN transceiver
Transceiver cuts number of required components by at least half in industrial applications
Bangalore (July 15, 2009) — Texas Instruments Incorporated (TI) today introduced the first isolated controller-area network (CAN) transceiver. The ISO1050 combines TI’s innovative CAN and isolation technologies to reduce required components by at least half, and simplifies board design in industrial automation, motor control and medical equipment. Loop time is reduced by 34 percent, giving designers flexibility to use longer network cables than can be used with other common isolated CAN solutions. For product details or to order samples, see: www.ti.com/iso1050pr-in.
“Customers are being challenged to design more complex industrial systems in smaller spaces,” said Art George, senior vice president of TI’s High-Performance Analog business unit. “The ISO1050 single-chip isolated CAN solution eases system design and allows engineers to reduce component count and speed time-to-market.”
Mr. Apoorva Awasthy, Business Development Manager, Analog, Texas Instruments India said, “The ISO1050 reduces system-level power consumption by 38 percent compared to isolated optocoupler solutions. In high-voltage applications where minimum clearance is required, the 6.1 mm wide-body package reduces board space by 30 percent. Additionally, the ultra-low electromagnetic emissions (EME) support sensitive analog applications, such as industrial sensors.”
Additional features and benefits
- The capacitive technology in TI isolators provides galvanic isolation of up to 4000 V and life expectancy of more than 25 years
- Meets requirements for the ISO 11898 standard
- Meets DeviceNet and CAN timing requirements
- Wide temperature range from –55C to 105C accommodates the requirements of a variety of industrial applications
- Customers can speed time-to-market with compatible TI devices including power isolation (DCR010505), and the Piccolo™ , Delfino™ and Stellaris® microcontroller series
Find out more about TI’s isolation portfolio by visiting the links below:
Order ISO1050 samples and evaluation modules: www.ti.com/iso1050-pr
See TI’s complete interface portfolio and selection guide: www.ti.com/interface-pr
Ask questions and share knowledge on TI’s E2E online community: http://www.ti.com/e2e-pr.
GE Security was honored with Frost & Sullivan’s 2008 North American Video Surveillance Solutions Company of the Year Award for its industry leading video portfolio and integration strategy vision and execution. For more information about GE Security, please visit www.gesecurity.com.
About Texas Instruments
Texas Instruments (NYSE: TXN) helps customers solve problems and develop new electronics that make the world smarter, healthier, safer, greener and more fun. A global semiconductor company, TI innovates through manufacturing, design and sales operations in more than 30 countries. For more information, go to www.ti.com.
Trademarks
All registered and other trademarks belong to their respective owners.
India Product Information Centre
Toll: +91-80-4138 1665
Toll free: +1-800-425-7888
GE Security EMEA
Email: tiasia@ti.com |