Placement Silo Title

News Releases

Media Coverage

Media Kit

Texas Instruments speeds ultrasound design and reduces board space by more than half with the first integrated transmit/receive switch

Bangalore (Oct. 6, 2009) – Texas Instruments Incorporated (TI) today introduced the industry’s first integrated, eight-channel, transmit/receive (T/R) switch for ultrasound systems. The TX810 addresses designers’ need to build smaller portable ultrasound systems, while speeding time to market [view video]. The TX810 integrates a protection diode bridge and clamp diodes for each of its eight channels to prevent the high-voltage pulses of the transmitter from damaging the receive electronics of the ultrasound system. The device saves more than 50 percent board space over discrete solutions in portable to mid-range ultrasound systems, and the component reduction and easier handling brings higher reliability to designs. For product details, please visit: www.ti.com/tx810-pr.

Key features and benefits of the TX810 T/R switch:

  • Eight integrated channels save more than 50 to 75 percent board space over discrete solutions, depending on T/R architectures
  • Integration allows for faster designs and higher reliability due to fewer devices and easier handling of components
  • Programmable bias currents allow designers to adjust and reduce power consumption:
    • 3-bit interface used to program a 7-mA range of bias currents
    • Power-down mode to reduce power consumption
  • Optimized insertion loss maintains integrity of input/output signal at 400Ω load with 0.9 dB at 7-mA bias current and 1.3 dB at 1-mA bias current
  • The TX810 completes TI’s signal chain offering for ultrasound systems together with the AFE58xx family of analog front ends, the TX734 high-voltage pulser and a broad portfolio of embedded processors for medical imaging, power management products, clocks and interfaces.

Learn more about TI’s full offering for ultrasound and other medical applications:

About medical components from Texas Instruments:

TI is helping shape technology to improve the quality and accessibility of medical equipment to revolutionize healthcare in the 21st century and beyond. With its full range of analog and embedded processing products, from building blocks to complete semiconductor solutions, plus systems insight, global support infrastructure, advanced process technology and medical industry involvement, TI is helping make innovative medical electronics more flexible, affordable and accessible. TI’s experience in diverse markets, such as wireless communications, consumer electronics, automotive and aerospace, enables engineers to meet increasing needs for higher speeds, higher precision, lower power and smaller equipment, while maintaining the high standards for quality and reliability that the medical market demands. For more information, please visit www.ti.com/medical.

About Texas Instruments:

Texas Instruments (NYSE: TXN) helps customers solve problems and develop new electronics that make the world smarter, healthier, safer, greener and more fun. A global semiconductor company, TI innovates through design, sales and manufacturing operations in more than 30 countries.  For more information, go to www.ti.com.

Trademarks

All registered trademarks and other trademarks belong to their respective owners.

India Product Information Centre

Toll: +91-80-4138 1665
Toll free: +1-800-425-7888
Email: tiasia@ti.com