Industry’s first passive low frequency interface with battery charge function from TI enables remotely powered medical, industrial and consumer products
New device wirelessly powers an MSP430™ MCU at ranges up to one meter
Bangalore (November 13, 2009) – Developers in medical, industrial and consumer applications continuously strive to increase wireless functionality to enhance the convenience of products. Texas Instruments (TI) today announced the industry’s first passive low frequency interface (PaLFI) device designed to wirelessly supply an ultra-low-power MSP430 microcontroller (MCU) with energy to operate even if the optional battery is empty. For example, PaLFI has the ability to remotely communicate with and power implantable medical devices, making procedures less invasive. Among numerous other potential applications, the device is also being used for production chain or container tracking and end of line configuration of electronic equipment such as CD/DVD players and measurement instruments. The device combines a low frequency wireless interface with an SPI interface which ensures ultra-stable communication within a very well defined activation/communication zone. For more information, visit www.ti.com/palfipr.
Key features and benefits of the PaLFI
- Battery check and charge function via RF field supports operation of hermetically sealed devices such as implants.
- PaLFI memory is accessible via an SPI and wireless LF 134 kHz interface allowing for access to additional microcontroller memory.
- The device can supply a battery powered MSP430 MCU with energy and operate the microcontroller even if the battery is empty ensuring data is still available and not getting lost.
- Low Frequency band (LF) ensures stable communication within a well defined reading zone.
- No battery required for data programming into the memory to allow an MCU to read content and use it for configuration, or calibration purposes once connected to the battery.
Find out more about TI’s new PaLFI device by visiting the links below:
About Texas Instruments:
Texas Instruments (NYSE: TXN) helps customers solve problems and develop new electronics that make the world smarter, healthier, safer, greener and more fun. A global semiconductor company, TI innovates through design, sales and manufacturing operations in more than 30 countries. For more information, go to www.ti.com.
Trademarks
All registered trademarks and other trademarks belong to their respective owners.
India Product Information Centre
Toll: +91-80-4138 1665
Toll free: +1-800-425-7888
Email: tiasia@ti.com |