Placement Silo Title

News Releases

Media Coverage

Media Kit

TI introduces fully-integrated load switch with lowest ON resistance

Bangalore (Dec. 16, 2009) – Texas Instruments Incorporated (TI) today introduced a fully-integrated load switch with typical ON resistance (rON) of 5.7-mΩ at 3.6-V, four times lower than the nearest competitor. TI’s TPS22924C integrates at least four parts into one to simplify subsystem load management. The high level of integration in an ultra-small 1.4-mm x 0.9-mm chip scale package (CSP) addresses space-constrained, battery-powered applications such as portable industrial and medical equipment, media players, point-of-sale terminals, global positioning systems (GPSs), notebooksnetbooks, and Smartphones. Download the datasheet and order samples at www.ti.com/tps22924c-pr.

Key features and benefits of the TPS22924C

  • Ultra-low ON resistance of 5.7-mΩ at 3.6-V offers minimum dropout through the pass FET.
  • Input voltage range of 0.75 V to 3.6 V supports portable applications.
  • 2-A maximum continuous switch current covers a wide range of currents.
  • Low shutdown current of <2uA uses minimum power consumption in shutdown mode.
  • The TPS22924C is the newest member of TI’s extensive load switch family. The new switch complements TI’s portfolio targeting the portable equipment market, which includes battery chargers, DC/DC converters and OMAP™ processors.

Find out more about TI’s load switch portfolio by visiting these links:

About Texas Instruments:

Texas Instruments (NYSE: TXN) helps customers solve problems and develop new electronics that make the world smarter, healthier, safer, greener and more fun. A global semiconductor company, TI innovates through manufacturing, design and sales operations in more than 30 countries. For more information, go to www.ti.com.

Trademarks

OMAP is a trademark of Texas Instruments. All registered trademarks and other trademarks belong to their respective owners.

India Product Information Centre

Toll: +91-80-4138 1665
Toll free: +1-800-425-7888
Email: tiasia@ti.com