TI’s new green phase-shifted full-bridge controller includes synchronous rectifier output control
Bangalore (Feb. 23, 2010) – Texas Instruments Incorporated (TI) today introduced a phase-shifted full-bridge PWM controller with synchronous MOSFET control outputs and light load power management. The UCC28950 can achieve efficiencies above 90 percentfrom light load to full load, enabling it to meet 90+ Climate Savers® efficiency standards. The device features a 10:1 wide range adaptive zero voltage switching (ZVS) control scheme. The wider ZVS operational range directly translates into reduced energy consumption across a wider power output range. For product details see: www.ti.com/ucc28950-prin
The UCC28950 also has optimized adaptive control for the output synchronous rectifiers including on/off control to optimize efficiency at lighter loads. The UCC28950 is designed for applications like high-power, high-density power supplies; server and telecom power supplies; industrial power systems; solar inverters; electric vehicles; and DC motor drives.
Key features and benefits of the UCC28950
- Synchronous rectifier outputs with optimized timing to minimize body diode conduction losses from typical propagation delays, which ensure high efficiency.
- UCC28950 features advanced power management functions that change operational modes under different start-up or load conditions and a burst mode that improves light load or no load efficiency by as much as 70 percent compared to non-green mode solutions. The UCC28950’s programmable ramp compensation allows for current or voltage mode control, adding system flexibility.
- A soft start with enable function allows the UCC28950 to initialize start-up by higher level system control.
- Sync in and sync out function with 90 degrees phase shift for interleaved operation of two parallel power supplies reduces input and output ripple current by 50 to 100 percent. This lower input and output ripple current allows designers to use smaller, lower-cost input and output capacitors.
Find out more about TI’s green controller portfolio at the links below:
About Texas Instruments:
Texas Instruments (NYSE: TXN) helps customers solve problems and develop new electronics that make the world smarter, healthier, safer, greener and more fun. A global semiconductor company, TI innovates through manufacturing, design and sales operations in more than 30 countries. For more information, go to www.ti.com.
Trademarks
Climate Savers is a trademark or registered trademark of World Wildlife Fund Inc., an international conservation organization. All other registered trademarks and other trademarks belong to their respective owners.
India Product Information Centre
Toll: +91-80-4138 1665
Toll free: +1-800-425-7888
Email: tiasia@ti.com |