Texas Instruments embraces Linux for C6x architecture
Bangalore (April 28, 2010) – Texas Instruments Incorporated (TI) (NYSE: TXN) today announced Linux kernel support for its C6x family of digital signal processors (DSPs) and multicore system-on-chips (SoCs) targeted for applications such as communications and mission critical infrastructure, medical diagnostics, and high-performance test and measurement. As customers move towards open source as a key element of their products, application developers can benefit from the availability of Linux on TI’s high-performance DSPs by having less software to develop, and focusing more on differentiating features and software in their applications.
“TI’s C6x-based processors have an enviable footprint in signal processing oriented high-performance multicore applications,” said Olaf Soentgen of Nash Technologies. “The introduction of Linux support expands the utility of the C6x into portions of these applications that traditionally have been reserved for RISC cores. We are taking advantage of Linux availability on TI’s SoC to lower the cost and simplify the development of femtocell base stations.”
TI’s C6x Linux effort is a community collaboration with considerable support already in place. As part of the effort to port the Linux kernel to the C6x ISA, Code Sourcery is developing a complete tool chain including support for the GNU Compiler Collection (GCC) and the GNU Project Debugger (GDB). The project’s goal is that both the C6x Linux kernel and the GCC / GDB tools will be accepted by kernel.org and the Free Software Foundation, making both fully supported as open source community projects. In addition, TI will sponsor a Linux-C6x portal and a community-oriented distribution program to facilitate communication and development around this technology. ENEA is making its open source, scalable multicore communications stack available to the C6x Linux community, as well as offering advanced multicore platform software and debugging tools. Nash Technologies is implementing features ranging from advanced chip level functions, such as multicore interprocessor communications, to complete LTE protocols. PolyCore Software, also an early community participant, is implementing the MCAPI multicore communications framework.
“Our customers are rapidly moving towards open source as a critical element of their solutions,” said Brian Glinsman, general manager of TI’s communications infrastructure business. “Because of the C6x-based products’ ultra low power consumption and cost effectiveness, customers are interested in running traditional DSP MAC/PHY and codec algorithms as well as classic RISC control code and protocols on our DSPs. TI’s embracing of Linux and an open tool chain for the industry workhorse C6x makes this kind of integration practical.”
Availability
Downloads of the C6x Linux kernel and GCC/GDB tools will be available in 3Q10.
For more information please visit the links below:
About Texas Instruments:
Texas Instruments (NYSE: TXN) helps customers solve problems and develop new electronics that make the world smarter, healthier, safer, greener and more fun. A global semiconductor company, TI innovates through design, sales and manufacturing operations in more than 30 countries. For more information, go to www.ti.com.
Trademarks
All trademarks are the property of their respective owners.
India Product Information Centre
Toll: +91-80-4138 1665
Toll free: +1-800-425-7888
Email: tiasia@ti.com |