TI introduces first high-performance Delfino™ floating-point microcontroller for extreme temperatures
Bangalore (April 21, 2011) – Texas Instruments Incorporated (TI) today introduced the industry’s first floating-point microcontroller (MCU) for extreme temperature operation from ‑55°C to 210°C. Exceeding the traditional 150°C limit for other high-temperature semiconductors, the SM320F28335-HT Delfino 32-bit MCU provides high-reliability, high-performance, real-time measurement and control for manufacturers of electronics operating in harsh and hot environments, such as downhole drilling, commercial jet engines, motor control, military applications, and medical instruments and surgical tools requiring sterilization.
The SM320F28335-HT Delfino MCU is based on TI’s popular TMS320C2000™ MCU platform, which combines control peripheral integration and embedded flash memory with the processing power of a 32-bit floating-point architecture. Enabling operation at up to 210°C eliminates the need for expensive up-screening and qualification tests of industrial grade MCUs, allowing for faster design of applications operating in harsh environments and cutting development time by up to one year. Packaging options, such as ceramic and Known Good Die (KGD), provide the smallest form factors for space-constrained applications.
“SM320F28335-HT Delfino MCU is first in the line of microcontroller products by TI’s High Reliability group which enables customers to meet specific high temperature requirements. It allows customers to use some of the latest designs from the TI High Temperature product portfolio ranging from amplifiers to complex embedded processors,” said Rakesh Joshi, General Manager - Business Development, HiRel Defense & Aerospace, Texas Instruments India
For complete product and tool information, visit www.ti.com/SM320F28335-HT-pr
Key features and benefits
- Operation from -55°C to 210°C for extreme temperature applications
- Integrated 32-bit floating-point unit with100-MHz CPU speed provides six times higher performance for real-time measurement and control than existing high-temperature solutions
- 512 KB of embedded flash memory and 68 KB internal RAM
- Integrated control-oriented peripherals to enable high precision
- Six high-resolution PWM outputs at 150 ps
- High-speed 16-channel 12-bit ADC
- Flexible packaging options to meet different environmental needs:
- High-temperature 181-pin ceramic PGA for 210°C operation
- KGD option for smallest package integration and multi-chip modules
- Plastic
Find out more about SM320F28335-HT and TI’s high-temperature products:
About high-reliability and high-temperature components from TI
Customers count on TI’s high-reliability expertise and the industry’s broadest portfolio of analog and embedded processing products to provide complete semiconductor solutions and value-added services for challenging or extreme environments in industrial, space, aerospace, defense, medical and consumer markets. TI offers solutions and services for extended temperature ranges for -55°C up to 220°C, radiation hardened designs, baseline control, extended product life cycles, obsolescence mitigation, quality conformance to military standards, ITAR flow support and in-house process technology. TI’s high-reliability packaging capabilities include ceramic, plastic and Known Good Die (KGD) wafer solutions. More at www.ti.com/hirel.
About Texas Instruments
Texas Instruments semiconductor innovations help 80,000 customers unlock the possibilities of the world as it could be – smarter, safer, greener, healthier and more fun. Our commitment to building a better future is ingrained in everything we do – from the responsible manufacturing of our semiconductors, to caring for our employees, to giving back inside our communities. This is just the beginning of our story. Learn more at www.ti.com.
Trademarks
Delfino, C2000 and TI E2E are trademarks of Texas Instruments. All registered trademarks and other trademarks belong to their respective owners.
India Product Information Centre
Toll: +91-80-4138 1665
Toll free: +1-800-425-7888
Email: tiasia@ti.com |