TI introduces 36-volt op amp for the automotive market
Micro package option is 50-percent smaller than competitive devices
Bangalore (September 22, 2011) – Texas Instruments Incorporated (TI) today introduced an automotive-qualified 36-V, single-supply, low-noise op amp (operational amplifier) that can operate on supplies ranging from +2.7 V to +36 V. The OPA171-Q1 offers high-precision performance in a cost-effective, low-power device. In addition to industry-standard packaging, the device is available for automotive qualification in the SOT-553 micro package, which is 50-percent smaller than comparable devices available today, and can reduce board space for automotive applications including HEV/EV, tracking amplifiers in power modules, and transducer amplifiers. For more information and to order samples, visit www.ti.com/opa171-q1-pr.
The OPA171-Q1 offers features designed to enhance overall system design stability, such as the ability to handle input signals beyond the supply rails without causing output phase reversal. The OPA171-Q1 remains stable when exposed to capacitive loads up to 300 pF or when the input operates 100 mV below the negative rail and within 2 V of the top rail during normal operation.
Key features and benefits of the OPA171-Q1:
- Dynamic input voltage range of +2.7 V to +36 V or ±1.35 V to ±18 V allows for greater design versatility across varying supply rails, while still enabling precise, low-voltage sensor outputs.
- The OPA171-Q1 provides precision performance, including low offset of up to 1.8 mV, typical drift of 0.3 uV/C and wide gain bandwidth of 3 Mhz.
- Low quiescent current of 475 uA enables efficient battery-powered operation.
- The SOT-553 micro package option uses 50-percent less board space than comparable op amps, which enables designers to develop smaller modules.
Tools and support
TI offers a variety of tools and support to speed the implementation of the OPA171-Q1 device:
Find out more about TI’s automotive and transportation portfolio by visiting the links below:
About Texas Instruments
Texas Instruments semiconductor innovations help 80,000 customers unlock the possibilities of the world as it could be – smarter, safer, greener, healthier and more fun. Our commitment to building a better future is ingrained in everything we do – from the responsible manufacturing of our semiconductors, to caring for our employees, to giving back inside our communities. This is just the beginning of our story. Learn more at www.ti.com.
Trademarks
TI E2E is a trademark of Texas Instruments. All other trademarks belong to their respective owners.
India Product Information Centre
Toll: +91-80-4138 1665
Toll free: +1-800-425-7888
Email: tiasia@ti.com |